2019-10-15 11:07 PM
2024-01-23 07:15 AM
I'm facing to the same problem. I tried to use hardware oversampling and offset but I could not get the good conversion.
As show in the previous post with some screenshot of the reference manual, I don't know if it's possible or not.
Please find also below, another sentence describing some restrictions on oversampling.
Finally my question: is it possible to use both oversampling and offset?
If yes, how to use it and what are exactly the restrictions?
Thanks in advanced for your help
2024-02-01 10:53 AM
Hello @Byann.1 ,
Please refer to the last release of RM0433 which contains update and correction.
The contradiction in the RM0433 Rev6 mentioned by waclawek.jan was already corrected in the Section: "Single ADC operating modes support when oversampling" to remove the mention that the offset correction is not supported in oversampling mode.