2023-10-18 1:01 AM - edited 2023-10-23 2:03 AM
Hi ST community,
For a project I would like to generate two interdependent PWM signals (Sa and Sw in the attached figure) with the STM32G0. The constraints/tasks are as follows:
The times for tSa,off and tSa,on are thus adjusted every 300us. The time tSw,on is limited cycle by cycle by the active break.
Following limitations I had to mention:
I will not present my previous approaches now, in order not to influence your ideas.
I look forward to your feedback.
Br, Stefan
Solved! Go to Solution.
2023-10-25 1:33 AM
But if I understand you correctly, your idea was to run the Sa with the combined PWM function and the Sw with the PWM2 mode. I have tried this and it works as well. Why do you prefer this approach? Because with this approach one register less has to be written?
Yes.
JW