2024-11-10 11:47 AM
Hi, I have an STM32303E-EVAL that I have been messing around with, but I also want to reset it to the demonstration functionality. I have downloaded the zip file for the demonstration firmware from the website, but I am not sure where to go from there. I tried to run the hex file in STM32CubeProgrammer, but that only made it ask for the sd card and didn't do anything further. Any help with what I need to do with the zip file would be appreciated.
2024-11-10 11:58 AM
But presumably if it had a MicroSD card with the media files on it, it wouldn't be asking for it..
2024-11-10 12:03 PM
When the sc card is in, it just stays on the white screen rather than running the demo. Thats why im not sure what im missing.
2024-11-10 12:06 PM
Hello @thomasgillen and welcome to the ST Community.
I suggest you to refer to the UM1851 specially the part 2.1.1 of it.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-10 12:09 PM
Let me go find the file you're talking about, and read the instructions, I'll get back to you..
It's a very old board, perhaps 12 years, and likely came with a 128MB card, not a current SDHC/SDXC one, so imagine a 2GB or smaller
The board doesn't look to have an External Loader for a NOR/NAND FLASH
2024-11-10 12:27 PM
Copy STM32303C-EVAL_FW_V1.0.0\Project\STM32303C-EVAL\Binary\Media on to the SDCard, so USER and STFILES at the top level
Use a 2GB card, or smaller
2024-11-10 12:42 PM
Thanks, but its the card that came with the board so those files were on the card by default. If it helps, I flashed it from a project where I selected the board and chose "Initialize all peripherals with their default mode." I thought that meant it would keep the demo but it didn't. After that, that's when I tried to run the hex file of STM32303C-EVAL_FW_V1.0.0 to get it back.