2023-05-19 7:26 AM
I'm having problems getting my software to work with FDCAN2 on the STM32G474e-EVAL board. It works with FDCAN1, but w/ FDCAN2, messages accumulate in the Tx buffer until I get buffer fill errors.
I built the FDCAN_Com_IT example from the latest STM32GCube firmware bundle and it fails in the exact same manner. Board is terminated correctly and I believe the CAN pins are wired to each other correctly. What could be going wrong here? Thanks.
-es
Solved! Go to Solution.
2023-07-03 9:03 AM
Ok, finally tracked this problem down. It would appear that some revisions of the STM32G474E-EVAL board default to having the FDCAN2 TX pin disconnected. If you solder the SB5 location on the board closed, the pin will be connected and FDCAN2 will work.
2023-05-19 8:50 AM
Hello,
Did you already test the example provided in STM32CubeG4 provided under the path Projects\STM32G474E-EVAL\Examples\FDCAN\FDCAN_Com_IT ? It uses FDCAN1 and FDCAN2. This is to ensure at least the HW part is OK...
2023-05-19 8:53 AM
Yes. The FDCAN_Com_IT application failed in the same manner (no transmission, buffer fill errors) when tested on two different STM32G474e-EVAL boards, so I'm reasonably sure it's not hardware or I've been profoundly unlucky.
-es
2023-05-19 8:58 AM
That's strange! I will try to run this example when I have this board on hands and get back to you for any feedback.
2023-05-19 8:59 AM
Thanks!
-es
2023-05-23 8:01 AM
Hi @ESchn.1 ,
I tested FDCAN_Com_IT example and I didn't find any issue.
Please make sure that :
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-23 8:18 AM
Hi Kaouthar,
Thank you for checking on this. I've definitely fitted jumpers JP1, JP2, and JP4 and correctly bridged FDCAN1 and FDCAN2, but I'm still seeing the same failure. What hash did you build the FDCAN_Com_IT example from?
-es
2023-05-23 8:29 AM
Hello @ESchn.1 ,
I built the FDCAN_Com_IT example from the last STM32CubeG4 1.5.1 package revision by using STM32CubeIDE 1.12.1 toolchain.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-23 8:40 AM
Ok, that looks like what I'm using as well. I've double checked the jumpers and tested the conductivity of the wires connecting FDCAN1 to FDCAN2 and they're good. Any idea what could be going wrong here to leave FDCAN1 working but FDCAN2 failing?
-es
2023-06-28 5:13 AM
I'm still experiencing this problem and have reproduced it on multiple boards. JP1, JP2, and JP4 are definitely set correctly and the CN12 and CN10 are correctly wired together. Is there anything else that could be causing this behavior? (Other jumpers, perhaps?) I'm currently powering the board via a Micro-USB plugged into a powered USB strip. (with JP-12 set for that.) Could this be a power issue? I've also tried powering via USB-C but behavior hasn't changed.