2024-07-23 05:13 AM
Dear All,
Currently I am trying to load some code to the STM32U599NJH6Q that is interfaced with the MT25QL128ABA QSPI flash over the OCTOSPI2 peripheral, using a JLink programmer.
The pinout of this peripheral on my custom PCB is:
I have also checked that I can read and write data to the flash, so the wiring should be fine.
Since I am using JLINK to program my device, I came across this information:
https://wiki.segger.com/J-Link_Multiple_Flashloader
So, based on this I modified my run script like this:
But I am getting this, when I am trying to download my app to the device:
Has anyone encountered something like this before? Any ideas or recommendations on what to do in order to fix it?
Thanks a lot in advance
2024-07-23 05:33 AM - edited 2024-07-23 06:56 AM
I'd assume there's not enough information passed for a "generic" loader to figure out it's on bank2, etc
I'd expect you'd still have to code something specific for your platform. Perhaps Segger has specific examples of this for other platform/chip options you can review.
https://wiki.segger.com/SEGGER_Flash_Loader
2024-07-23 05:53 AM
@Tesla DeLoreanthanks for your reply.
Could you elaborate a bit more on what steps do I need to take here?
2024-07-23 07:03 AM
Review how Segger implements on other STM32 platforms like the H743
See how it works for other platforms, see the code or scripting used / provided
Confer with Segger support and their documentation. Do they provide any U5 or U575 examples?
Not sure if CubeIDE can use J-Link and push in .STLDR External Loaders for ST-LINK. The mechanics there is to put the loader in available RAM, and call functional entry points. That's a pretty standard/common method to do that. Keil uses FLM. IAR/EWARM is a little more scripted.
Second bank OSPI/QSPI on the U5 would need specific code and AF relationships for the pins, and that's not exactly consistent between STM32 models, or U5 members either.
2024-07-23 07:10 AM
Do you have a pointer on where to start with reviewing the solutions they offer?
I have not been able to find much so far.
Where can I see the default configurations for a specific board? Is it part of the STM32CubeIDE plugins folder?