2022-07-07 8:44 AM
Hi all.
I'm trying to run external mode simulation using:
I have created a simple LED example to test the external mode and I used the Embedded Coder to integrate it with the CubMX Project file. The problem is when i'm trying to run in external mode, I can't do it because the Monitor&Tune button is grayed out and I can't press it. In the Hardware Implementation settings, I have checked the External Mode at the Interface section. Could you guys please help me where I went wrong?
Thanks a lot.
2022-07-07 9:14 AM
Again, you need to be referring Simulink & Matlab questions to Mathworks: