Skip to main content
MArvi.1
Associate II
Jul 6, 2022 9:00 AM UTC
Question

How do I configure STM32-L476RG and use the Timer(Encoder Mode/PWM) in Matlab-Simulink?

Hi all,

I am trying to program and control a Reaction Wheel Inverted Pendulum in real-time with a STM32-L476RG board and a SimpleFOCShield using Simulink. But first, I wanted to see whether I can read the incoming encoder values in Simulink through the STM32-L476RG. I have installed the STM32 Support Packages, but it doesn't really fulfill my needs. For example, I want to read the values of an encoder or generate PWM with STM32 in Simulink, there are no blocks for the Timer, which has the encoder mode function. And I can't upload/connect the configuration of the pins from STM32CubeMX for the board I am using. I am quite new to STM32, so I am wondering if there are solutions/alternatives/suggestions to this?

Thank you very much.

0693W00000QKXrvQAH.png 

0693W00000QKXs0QAH.png

This topic has been closed for replies.

3 replies

Andrew Neil
Super User
Jul 6, 2022 9:09 AM UTC

Simulink & Matlab are independent 3rd-party products - nothing to do with ST.

Also not widely used here, I suspect.

You really need to go to Mathworks support for help with their products:

https://uk.mathworks.com/support.html

"it doesn't really fulfill my needs"

So is there really any benefit in using it over the "normal" microcontroller development tools?

It's always going to be the problem with these "canned" solutions - when you want to do stuff that's a bit off their idea of the "usual" application...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MArvi.1
MArvi.1Author
Associate II
Jul 6, 2022 9:23 AM UTC

Okay thank you for your answer.

vchilapu
Associate II
Jul 7, 2022 12:42 PM UTC

The Simulink Coder Support Package for STM32 is based on the ARM mbed. Since mbed does not have support for the Encoder, MATLAB/Simulink doesn't have a block for the same either. You can try connecting with MathWorks paid consulting for the same.