cancel
Showing results for 
Search instead for 
Did you mean: 

Ext. Interrupt conflict on STM32H7 ?

HMSEdinburge
Associate II

Hello, I'm using H723 Nucleo. I set 5 ext interrupt pins: PA0, PA1, PA4, PC2_C, and PC13 as EXTI to 5 switches, enabled NVIC interrupt, GPIO pull-up,  interrupt with rising edge triggered, and tied these 5 pins to switches with the other end to ground. The code is working fine, but I observe that only 1 interrupt (either 1 of the 5 switches) can work at any one time, and all 5 interrupts cannot work together at any instance... is this interrupt conflict on H7? Anyone can advise? 

 

 

if (GPIO_Pin == GPIO_PIN_0)
	{
		// on LED1
	}

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello @HMSEdinburge ,

First, I have remarks regarding the info you provided:


@HMSEdinburge wrote:

enabled NVIC interrupt, GPIO pull-up,  interrupt with rising edge triggered,

 

 -> You set pull up and you set the EXTI edge to rising which is not correct. You need either to set pull-up resistor and set the edge to falling or set pull-down resistor and set the edge to rising.


@HMSEdinburge wrote:

Hello, I'm using H723 Nucleo. I set 5 ext interrupt pins: PA0, PA1, PA4, PC2_C, and PC13

 

PA1 is connected to the ETH PHY RMII_REF_CLK pin on the board. need to select another pin. PC13 is used by the user button which has already an external pull-down resistor. So no need to set pull up/down internal resistor.

Now regarding the code, this is how it could be managed:

 

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
  switch(GPIO_Pin)
  {
    case GPIO_PIN_0:  exti_source  = 1; break; // PA0
    case GPIO_PIN_3:  exti_source  = 2; break; // PA3 instead of PA1
    case GPIO_PIN_4:  exti_source  = 3; break; // PA4
    case GPIO_PIN_2:  exti_source  = 4; break; // PC2_C 
    case GPIO_PIN_13: exti_source  = 5; break; // PC13
    default: exti_source= 0; break;
  }
}

 

I've attached a project running on NUCLEO-H723 that uses all these EXTIs (just replaced PA1 by PA3) . Put exti_source in live watch and you can see the value that changes according to the EXTI event triggered.

Hope that answers your question.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

View solution in original post

4 REPLIES 4
Sarra.S
ST Employee

Hello @HMSEdinburge,

Make sure that each EXTI line is configured for the respective GPIO pins, each pin should be assigned to a unique EXTI

Also, could share some code? 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi i had checked and re-check the Pins assignment as screenshot and code below:

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
	if (GPIO_Pin == Btn1_Pin)  // PIN_0
	{
		// LED1 on
	}

	else if (GPIO_Pin == GPIO_PIN_1)  
	{
		// LED2 ON
	}

	else if (GPIO_Pin == Btn2_Pin) 
	{
		// LED 3 ON
	}

	else if (GPIO_Pin == Btn3_Pin)
	{
		// LED3 ON;
	}

	else if (GPIO_Pin == GPIO_PIN_13)
	{
		// LED 4 ON
	}
}

below, 

GPIOa.jpggpioB.jpg

SofLit
ST Employee

Hello @HMSEdinburge ,

First, I have remarks regarding the info you provided:


@HMSEdinburge wrote:

enabled NVIC interrupt, GPIO pull-up,  interrupt with rising edge triggered,

 

 -> You set pull up and you set the EXTI edge to rising which is not correct. You need either to set pull-up resistor and set the edge to falling or set pull-down resistor and set the edge to rising.


@HMSEdinburge wrote:

Hello, I'm using H723 Nucleo. I set 5 ext interrupt pins: PA0, PA1, PA4, PC2_C, and PC13

 

PA1 is connected to the ETH PHY RMII_REF_CLK pin on the board. need to select another pin. PC13 is used by the user button which has already an external pull-down resistor. So no need to set pull up/down internal resistor.

Now regarding the code, this is how it could be managed:

 

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
  switch(GPIO_Pin)
  {
    case GPIO_PIN_0:  exti_source  = 1; break; // PA0
    case GPIO_PIN_3:  exti_source  = 2; break; // PA3 instead of PA1
    case GPIO_PIN_4:  exti_source  = 3; break; // PA4
    case GPIO_PIN_2:  exti_source  = 4; break; // PC2_C 
    case GPIO_PIN_13: exti_source  = 5; break; // PC13
    default: exti_source= 0; break;
  }
}

 

I've attached a project running on NUCLEO-H723 that uses all these EXTIs (just replaced PA1 by PA3) . Put exti_source in live watch and you can see the value that changes according to the EXTI event triggered.

Hope that answers your question.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

yes, i m using PC13 on-board switch, I'll try your code and suggestion...