cancel
Showing results for 
Search instead for 
Did you mean: 

Evaluate STM32L071xx on STM32L073RZ development board

Harry Tsang
Associate II
Posted on June 19, 2018 at 05:11

Hi everyone, could I purchase 

STM32L073RZ development board to evaluate STM32L071xx?  Actually I will start with some code for STM32L071xx generated by STM32CubeMX and then download into the

 development board, could

STM32L073RZ

perform the same as the actual MCU (STM32L071xx) I am going to use in final product?  Many thanks!

#stm32l073rz #stm32l071
4 REPLIES 4
Posted on June 19, 2018 at 10:28

Could

STM32L073RZ

perform the same as the actual MCU (STM32L071xx) I am going to use in final product?

Yes, except of course those modules which represent the difference between 'L073 and 'L071.

JW

Posted on June 19, 2018 at 14:36

All STM32L07 have the same die. Compile for the

STM32L071

and run on

STM32L073

and things the chip will behave the same as a 'real'

STM32L071

Posted on June 20, 2018 at 03:25

Thanks for your reply

Posted on June 20, 2018 at 03:26

Thanks for your reply