cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f746disc sdmmc with fatfs make problem while read or open file in 4 bit mode

egywell
Associate II
Posted on March 06, 2017 at 04:26

I use fatfs to read text file line by line every time 

when i use normal sdmcc driver which initialize sd wide mode to 4 B  i got fault errors randomly and fatfs hang or stuck at hal sd_getscr function

so i have to change driver setting to 1B mode

I searched too much but couldnot find the problem solution 

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on March 06, 2017 at 08:35

Dear elbeshlawy.mohammed,

Try to reduce SDMMC clock(down to below 12MHz),use FIFO Polling instead of DMA and insert series resistor on SDMMC_CK line(nearby MCU side).

Posted on March 06, 2017 at 11:44

Thanks for reply

I enabled hardware flow control then problem solved with 4 bit mode 

Is that enough or still I have to do what you advised ?

Posted on March 06, 2017 at 12:45

I reduced clk to 16 mhz also problem solved without enable hardware control which mean I have to thank you very much 

Bob Feretich
Associate
Posted on June 20, 2018 at 07:37

If reducing the clock to 16 MHz fixed the problem, then...

Verify that STM32F7 I/O compensation was turned on.

Verify that all the SDIO interface pins were set to 'fast' (50 MHz) edge speeds. They default to 2MHz.