2018-06-18 08:11 PM
Hi everyone, could I purchase
STM32L073RZ development board to evaluate STM32L071xx? Actually I will start with some code for STM32L071xx generated by STM32CubeMX and then download into the
development board, could
STM32L073RZ
perform the same as the actual MCU (STM32L071xx) I am going to use in final product? Many thanks!#stm32l073rz #stm32l0712018-06-19 01:28 AM
Could
STM32L073RZ
perform the same as the actual MCU (STM32L071xx) I am going to use in final product?Yes, except of course those modules which represent the difference between 'L073 and 'L071.
JW
2018-06-19 07:36 AM
All STM32L07 have the same die. Compile for the
STM32L071
and run onSTM32L073
and things the chip will behave the same as a 'real'STM32L071
2018-06-19 08:25 PM
Thanks for your reply
2018-06-19 08:26 PM
Thanks for your reply