2023-12-18 3:25 AM
When ever i am trying to copy data in SDRAM garbage value is getting transferred. Please suggest what can i do
I have attached necessary files with this post.
Kindly suggest.
Solved! Go to Solution.
2024-01-04 5:33 AM - edited 2024-01-04 6:35 AM
Hello @Rushali ,
--> unable to change command mode value after sending commands.
Thank you for bringing this issue to our attention.
After checking, I confirm that the MODE Bits read as zero after the command is issued and this is normal behavior.
The MODE bits are write only. For that I reported the reference manual internally for correction.
Internal ticket number: 169917 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-18 7:22 AM
Hello @Rushali and welcome to the Community :),
Please make sure that the timing parameters are set correctly.
I think that How to set up the FMC peripheral to interface with the SDRAM IS42S16800F-6BLI from ISSI FAQ can help you.
Also, you can start by an available example such as FMC_SDRAM_DataMemory and get inspired to configure your project.
Note that, this example has been tested with STM32H747I-EVAL board with SMPS (SD Converter) power supply config when the SDRAM is IS42S32800G, but can be easily tailored to any other supported device and development board.
I hope this help you!
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-19 5:12 AM
Thank you for your reply.But i have narrowed down the problem.i found out that while initalizing SDRAM with FMC i have written following code.
void FMC_INIT(void) {
HAL_StatusTypeDef status;
/* Step 1 and Step 2 already done in HAL_SDRAM_Init() */
/* Step 3: Configure a clock configuration enable command */
Command.CommandMode = FMC_SDRAM_CMD_CLK_ENABLE; /* Set MODE bits to "001" */
Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2 ; /* configure the Target Bank bits */
Command.AutoRefreshNumber = 3;
Command.ModeRegisterDefinition = 0;
/* while (FMC_GetFlagStatus(FMC_Bank2_SDRAM, FMC_FLAG_Busy) != RESET) {
}*/
/* Send the command */
status = HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff);
HAL_Delay(1); /* Step 4: Insert 100 us minimum delay - Min HAL Delay is 1ms */
/* Step 5: Configure a PALL (precharge all) command */
Command.CommandMode = FMC_SDRAM_CMD_PALL; /* Set MODE bits to "010" */
HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff);
/* Step 6: Configure an Auto Refresh command */
Command.CommandMode = FMC_SDRAM_CMD_AUTOREFRESH_MODE; /* Set MODE bits to "011" */
Command.AutoRefreshNumber = 2;
HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff);
/* Step 7: Program the external memory mode register */
Command.CommandMode = FMC_SDRAM_CMD_LOAD_MODE;/*set the MODE bits to "100" */
Command.ModeRegisterDefinition = (uint32_t)0 | 0<<3 | 2<<4 | 0<<7 | 1<<9;
HAL_SDRAM_SendCommand(&hsdram1, &Command, 0xfff);
/* Step 8: Set the refresh rate counter - refer to section SDRAM refresh timer register in RM0455 */
/* Set the device refresh rate
* COUNT = [(SDRAM self refresh time / number of row) x SDRAM CLK] – 20
= [(64ms/4096) * 100MHz] - 20 = 1562.5 - 20 ~ 1542 */
HAL_SDRAM_ProgramRefreshRate(&hsdram1, 733);
}
But unable to change command mode value after sending commands.
2024-01-04 5:33 AM - edited 2024-01-04 6:35 AM
Hello @Rushali ,
--> unable to change command mode value after sending commands.
Thank you for bringing this issue to our attention.
After checking, I confirm that the MODE Bits read as zero after the command is issued and this is normal behavior.
The MODE bits are write only. For that I reported the reference manual internally for correction.
Internal ticket number: 169917 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.