2024-05-22 07:16 AM
Error: Mass erase operation failed.Please verify flash protection stm32h5 board
I faced this while erasing external memory from programmer
I find a solution related to st-link-utility but this program doesn`t support h5 boards Solved: STM32F722ZE Error: Mass erase operation failed. Pl... - STMicroelectronics Community
Solved! Go to Solution.
2024-05-23 04:32 AM - edited 2024-05-23 08:13 AM
Hello @Ahmed_hassan and welcome to the Community :),
Thank you @Tesla DeLorean for your contribution in STComminty and for bringing issue to our attention.
Which board revision are you using?
If you have a STM32H573I-DK-RevA board , please use MX25LM51245G_STM32H573I-DK.
If you have other boards revisions like as RevB or RevC, please use MX25LM51245G_STM32H573I-DK-RevB.
Please let me know if the issue is solved or not?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-22 08:15 AM
Please provide more detail of the exact board configuration, external memory, and external loader.
Provide logs from STM32 Cube Programmer, with Verbose Level 3
2024-05-22 08:24 AM
2024-05-23 04:32 AM - edited 2024-05-23 08:13 AM
Hello @Ahmed_hassan and welcome to the Community :),
Thank you @Tesla DeLorean for your contribution in STComminty and for bringing issue to our attention.
Which board revision are you using?
If you have a STM32H573I-DK-RevA board , please use MX25LM51245G_STM32H573I-DK.
If you have other boards revisions like as RevB or RevC, please use MX25LM51245G_STM32H573I-DK-RevB.
Please let me know if the issue is solved or not?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-23 07:41 AM
It works thank you for helping.