cancel
Showing results for 
Search instead for 
Did you mean: 

During the test, we found that the reference voltage of DAC channel 1 for STM32L4P5is 3V,while the VREFBUF for channel 2 is 2.048V,they are not identical,and the VREFBUF->CSR value is 2.

HAlex.1
Associate II
 
4 REPLIES 4

And what's the actual voltage on VREF+ pin? Don't you have connected 3V to it externally?

You may also want to read https://community.st.com/s/article/how-to-configure-vrefbuf-on-my-stm32

JW

Yes, the VREF is connected to 3V externally.

We found that if the DAC output is connected with a 100K resistor, it is 3V, while if it is connected to a 27K resistor , the output is lowered to 2V. Does it because of the driver?

What do you mean by "driver"?

The DAC's current driving capability is small, see datasheet. You can switch on a buffer, but then the output won't go all the way to the rails.

JW