Browse
STMicroelectronics Community
FAQs
Sign In
Product forums
STM32 MCUs
STM32 MCUs products
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
STM32 MCUs Other solutions
STM32 MPUs
STM32 MPUs products
STM32 MPUs Boards and hardware tools
STM32 MPUs Software development tools
STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
Microcontrollers
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
HAlex.1
Associate II
since
2020-09-24
2023-06-14
User statistics
4
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About HAlex.1
Options
Report User
User Activity
Posts
Replies
During the test, we found that the reference voltage of DAC channel 1 for STM32L4P5is 3V,while the VREFBUF for channel 2 is 2.048V,they are not identical,and the VREFBUF->CSR value is 2.
2022-01-20
Does the PSSI accept to be used in master mode? How to set it?
2021-07-05
Re: During the test, we found that the reference voltage of DAC channel 1 for STM32L4P5is 3V,while the VREFBUF for channel 2 is 2.048V,they are not identical,and the VREFBUF->CSR value is 2.
2022-01-22
We found that if the DAC output is connected with a 100K resistor, it is 3V, while if it is connected to a 27K resistor , the output is lowered to 2V. Does it because of the driver?
Re: During the test, we found that the reference voltage of DAC channel 1 for STM32L4P5is 3V,while the VREFBUF for channel 2 is 2.048V,they are not identical,and the VREFBUF->CSR value is 2.
2022-01-22
Yes, the VREF is connected to 3V externally.