cancel
Showing results for 
Search instead for 
Did you mean: 

Are there any DISCO or EVAL boards for STMH7 MPUs that offer access to an unused I2C bus for external peripherals?

SNort.1
Associate II

I might be missing a trick here, but it seems that most (if not all) DISCO / EVAL boards expose the same I2C bus externally that is used to communicate with onboard peripherals.

This makes perfect sense with DISCO boards as they are small / low cost. But I had hoped that on the EVAL boards there might be an option for one of the free I2C busses to be exposed. And to be able to dedicate one I2C bus to the M4 and another to the M7, for example.

I don't seem to be able to find one with an alternate pin function set that allows this. Am I missing something obvious?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
S.Ma
Principal

Eval boards have jumpers to disconnect external transceiver, so there should be options there. Or use the poor man's sw bit bang solution, in this case many gpio candidates....

DISCO / NUCLEO boards would probably expose via the ARDUINO SHIELD, run OLEDs and GNSS receivers from there,and on H7 board

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..