cancel
Showing results for 
Search instead for 
Did you mean: 

Does the STM32G070CBT6 have a Unique ID?

stst9191
Associate II

In spite to the reference manual of the STM32G071CBT6 the unique ID is not described in the reference manual of the STM32G0x0 series, but its address is defined in the header file (stm32g070xx.h).

Now I wonder if it is missing in the reference manual or if the header file is wrong.

Does someone know if the STM32G070CBT6 has the unique ID (UID_BASE)?

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @stst9191​ ,

I asked the same question here

https://community.st.com/s/question/0D53W00001rtbuOSAQ/rm0454-chapter-30-is-missing-uid-information

Unfortunately ST official answer is that the UID that you can read is not really unique, for costs reasons.

Best regards

View solution in original post

4 REPLIES 4
Imen.D
ST Employee

Hello @stst9191​ ,

>In spite to the reference manual of the STM32G071CBT6 the unique ID is not described in the reference manual

Do you mean STM32G070CBT6 and not STM32G071CBT6?

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
stst9191
Associate II

Hello Imen,

I mean the STM32G070CBT6.

Stefan Zimmer

Hi @stst9191​ ,

I asked the same question here

https://community.st.com/s/question/0D53W00001rtbuOSAQ/rm0454-chapter-30-is-missing-uid-information

Unfortunately ST official answer is that the UID that you can read is not really unique, for costs reasons.

Best regards

stst9191
Associate II

Hi Kraal,

thank you for this information.

Best regards