cancel
Showing results for 
Search instead for 
Did you mean: 

RTC not working correctly with octoSPI(stm32h723)

Mtopa.1
Associate II

Hello everybody.

I want to ask a question about a project. In my project, when octoSPI and RTC work together, an error occurs (counting incorrectly) in RTC's counting and it starts to count slower, but when I turn off octoSPI, RTC starts counting correctly. What do you think could be the reason?

The processor I am using is STM32h723vet6

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello @Mtopa.1​ ,

Check your HyperRam and make sure to configure the memory properly.

You can share your configuration this will help users Community to answer you.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Mtopa.1
Associate II

Hello Imen DAHMEN (ST Employee),

My ram configuration is as follows.

i am using APS6408L-3OBM-BA ram

OSPIM_CfgTypeDef OSPIM_Cfg_Struct = {0};

 OSPI_RegularCmdTypeDef sCommand;

 OSPI_MemoryMappedTypeDef sMemMappedCfg = {0};

 OSPIHandle.Instance = OCTOSPI1;

 HAL_OSPI_DeInit(&OSPIHandle);

 OSPIM_Cfg_Struct.ClkPort = 1;

 OSPIM_Cfg_Struct.DQSPort = 1;

 OSPIM_Cfg_Struct.NCSPort = 1;

 OSPIM_Cfg_Struct.IOLowPort = HAL_OSPIM_IOPORT_1_LOW;

 OSPIM_Cfg_Struct.IOHighPort = HAL_OSPIM_IOPORT_1_HIGH;

 if (HAL_OSPIM_Config(&hospi1, &OSPIM_Cfg_Struct, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

 {

  Error_Handler();

 }

  

 OSPIHandle.Init.FifoThreshold     = 1;

 OSPIHandle.Init.DualQuad       = HAL_OSPI_DUALQUAD_DISABLE;

 OSPIHandle.Init.MemoryType      = HAL_OSPI_MEMTYPE_APMEMORY;

 OSPIHandle.Init.DeviceSize      = 23; /* 256 MBits */

 OSPIHandle.Init.ChipSelectHighTime  = 1;

 OSPIHandle.Init.FreeRunningClock   = HAL_OSPI_FREERUNCLK_DISABLE;

 OSPIHandle.Init.ClockMode       = HAL_OSPI_CLOCK_MODE_0;

 OSPIHandle.Init.WrapSize       = HAL_OSPI_WRAP_NOT_SUPPORTED;

 OSPIHandle.Init.ClockPrescaler    = 2;//3;

 OSPIHandle.Init.SampleShifting    = HAL_OSPI_SAMPLE_SHIFTING_NONE;

 OSPIHandle.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;

 OSPIHandle.Init.ChipSelectBoundary  = 10;

 OSPIHandle.Init.FreeRunningClock   = HAL_OSPI_FREERUNCLK_ENABLE;

 OSPIHandle.Init.DelayBlockBypass   = HAL_OSPI_DELAY_BLOCK_USED;//HAL_OSPI_DELAY_BLOCK_BYPASSED;

 OSPIHandle.Init.Refresh = 0xFFFF;

  

  

  if (HAL_OSPIM_Config(&OSPIHandle, &OSPIM_Cfg_Struct, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

 {

  Error_Handler();

 }

 if (HAL_OSPI_Init(&OSPIHandle) != HAL_OK) {

  Error_Handler();

 }

  

  

 if (HAL_OSPI_Init(&OSPIHandle) != HAL_OK)

 {

  Error_Handler() ;

 }

  __HAL_OSPI_DISABLE(&OSPIHandle);

 HAL_Delay(100);

 CLEAR_BIT(OSPIHandle.Instance->DCR1, OCTOSPI_DCR1_FRCK);

 __HAL_OSPI_ENABLE(&OSPIHandle);

 HAL_Delay(1000);

  

 sCommand=read_reg(sCommand);

 if (HAL_OSPI_Command(&OSPIHandle, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

 {

  Error_Handler();

 }

 if (HAL_OSPI_Receive(&OSPIHandle, MR_R, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

 {

  Error_Handler();

 }

 //-----------write Register------------

  

  sCommand=write_reg(sCommand);

  if (HAL_OSPI_Command(&OSPIHandle, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

  {

   Error_Handler();

  }

  if (HAL_OSPI_Transmit(&OSPIHandle, MR_write, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

  {

   Error_Handler();

  }

  

 sCommand.Instruction    = WRITE_CMD_SRAM;

 sCommand.OperationType   = HAL_OSPI_OPTYPE_WRITE_CFG;

 sCommand.NbData       = 10;

 sCommand.DummyCycles    = DUMMY_CLOCK_CYCLES_SRAM_WRITE;

 if (HAL_OSPI_Command(&OSPIHandle, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) {

  Error_Handler();

 }

 sCommand.OperationType = HAL_OSPI_OPTYPE_READ_CFG;

 sCommand.Instruction  = READ_CMD_SRAM;

 sCommand.DummyCycles  = DUMMY_CLOCK_CYCLES_SRAM_READ;

 if (HAL_OSPI_Command(&OSPIHandle, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) {

  Error_Handler();

 }

 sMemMappedCfg.TimeOutActivation = HAL_OSPI_TIMEOUT_COUNTER_DISABLE;

 if (HAL_OSPI_MemoryMapped(&OSPIHandle, &sMemMappedCfg) != HAL_OK) {

  Error_Handler();

 }