2024-03-29 10:27 AM
Hi,
when I tried to set the clock of I3C which is 12.5Mhz, it didn't work properly.
Do I need something else to have 12.5mhz frequency?
Thanks,
Luke.
2024-03-29 12:50 PM
Dear @LukeJang522 ,
Here is a tutorial on I3C step by step .
https://wiki.st.com/stm32mcu/wiki/Getting_started_with_I3C
if you can share your system clocks and a screenshot to help .
Cheers,
STOne-32
2024-03-29 1:18 PM
Hi,
the tutorial that you sent, I3C frequency setting is 3000khz.
I tried 12500KHz, but it didn't work. I wasn't even able to transmit the data.
Thanks.
2024-03-29 8:26 PM
Hi @LukeJang522 ,
Can you share your I3C configuration if set in push-pull mode as example ?
some details are in this Application Note - Section 6 : https://www.st.com/resource/en/application_note/an5879-introduction-to-i3c-for-stm32h5-series-mcu-stmicroelectronics.pdf
Let me know
STOne/32
2024-04-01 11:02 AM - edited 2024-04-01 11:03 AM
Please see the below screen shot.
I tried 3000Khz, I3C communication is working well but clock is lower than 3Khz.
below screen shot is for 3000Khz.
2024-04-02 7:30 AM
Hello @LukeJang522 ,
Could you please specify your target : sensor , stm32h5 , .. ?
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-02 2:18 PM
Foued_KH,
My target board is X-NUCLEO-IKS02A1. I was going to try with IKS01A3, but it was out of stock.
Do you think there might be some problem?
but I can see the data communication by scope when I tried 3000Khz.
Thanks.
Luke.
2024-04-03 1:48 AM
I don't think that X-NUCLEO-IKS02A1 supports sensors with I3C interface .
You can use X-NUCLEO-IKS01A3 ( LSM6DSO , LPS22HH ) or X-NUCLEO-IKS4A1 and for more details about I3C sensor communication, check this path :
STM32Cube_FW_H5_V1.2.0\Projects\NUCLEO-H533RE\Examples\I3C\I3C_Sensor_Private_Command_IT ( X-NUCLEO-IKS4A1)
STM32Cube_FW_H5_V1.2.0\Projects\NUCLEO-H503RB\Examples\I3C\I3C_Sensor_Private_Command_IT (X-NUCLEO-IKS01A3)
Thank you!
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.