2020-03-26 12:05 PM
The information in the reference manual (RM0440) is very limited.
There is an app note: "AN5224 DMAMUX description" but it says it only covers STM32H7, STM32G0, STM32L4+ and STM32WB series.
Also, if you search the resources for the STM32G474 this application note doesn't come up.
Can you confirm that this application note applies? If not, point to more details?
Thanks.
2020-03-26 2:15 PM
IMO it does apply, it's just that nobody updated it, and also nobody cared enough to add it into the 'G4 folders' resources.
JW
@Vincent Onde , can please this AN be updated and added to the 'G4 folders' resources?
2020-03-27 1:10 AM
Hello All,
I raised your feedkack internally to the Doc owner to take in consideration and update the AN.
Best Regards,
Imen