cancel
Showing results for 
Search instead for 
Did you mean: 

Correction Request: Inconsistent usage of terms in AN2867 (Oscillator Design Guidelines)

BarryWhit
Senior III

It is vital to use language and terms with great care and  precision in technical writing. Whenever you don't, you create confusion.

 

Newcomers often make the mistake of conflating the terms "crystal", and "oscillator". For example, see @Andrew_Neil   's multiple comments on this thread, where he does his utmost to banish this common error.

Quite recently, I made the same mistake when asking for help finding a low-power clock source.

 

We can forgive newcomers and ourselves our trespasses (I personally have, grudgingly), but shouldn't we expect more from official ST documentation?

 

AN2867: Guidelines for oscillator design on STM8AF/AL/S and STM32 MCUs/MPUs

mixes and shifts between related terms multiple times in its 59 pages. The resulting confusion is enormous. Instead of working to remove confusion, ST's documentation contributes to it:

osc1.jpg

==

osc2.jpg

==

osc3.jpg

==

OSC4.jpg

==

OSC5.jpg

==

OSC6.jpg

which is followed immediately by

OSC7.jpg

==

OSC9.jpg

 

Dear ST,  please flag this AN for review and urge the documentation team to be absolute tyrants about correct usage.

- If a post has answered your question, please acknowledge the help you received by clicking "Accept as Solution".
- Once you've solved your issue, please consider posting a summary of any additional details you've learned. Your new knowledge may help others in the future.
8 REPLIES 8
BarryWhit
Senior III

From [EPSON] Crystal Fundamentals & State of the Industry :

OSC10.jpg

 

If ST writers lack a catch-all term, perhaps "Frequency Source" would do, instead of randomly selecting one of the three (crystal, oscillator, resonator) on each occasion. Including a glossary placed at the start of the appnote would enhance clarity as well.

- If a post has answered your question, please acknowledge the help you received by clicking "Accept as Solution".
- Once you've solved your issue, please consider posting a summary of any additional details you've learned. Your new knowledge may help others in the future.
STOne-32
ST Employee

Dear @BarryWhit @Andrew Neil ,

 

Thank you for the feedback. I concur your message and Will be taken into account in our next Release . Indeed nowadays “resonators” are rarely used IMHO as most of modern MCUs have very nice RC / HSI / MSI precision low cost internal oscillators , this was not the case 20 years ago where they are very famous and especially from Murata. As we work with many crystal partners we have close contact with all of them and major breakthrough the last decade was : Ultra low power and very small PCB footprint to reach 1016 and even lower size while keeping very high precision including Wireless communications and asynchronous clocking : Ethernet, USB etc.

well received for the AN2867 ! 

Cheers,

STOne-32

BarryWhit
Senior III

So... no internal ticket for this?

 

This term confusion is an engineering epidemic. ST should make an effort to stop this confusion by explicitly calling this common error out in documentation, and should also avoid making it themselves in their literature.

 

From SE:

OSC11.jpg

- If a post has answered your question, please acknowledge the help you received by clicking "Accept as Solution".
- Once you've solved your issue, please consider posting a summary of any additional details you've learned. Your new knowledge may help others in the future.
STOne-32
ST Employee

Dear @BarryWhit ,

>>So... no internal ticket for this? >>

The door is already open ;-).  let's close it with AN2867 Update on next release and may be also a Knowledge Article on the topic that covers crystals, oscillators.  For follow-up the internal number is #185375.

Wish you a great sunday.

Ciao

STOne-32.

 

Thank you, @STOne-32 . Fingers crossed.

- If a post has answered your question, please acknowledge the help you received by clicking "Accept as Solution".
- Once you've solved your issue, please consider posting a summary of any additional details you've learned. Your new knowledge may help others in the future.

@BarryWhit wrote:

crystal, oscillator, resonator


I'd say that "resonator" is a generic term which includes both crystal resonators and ceramic resonators - maybe even RC and LC ...

But, whatever, the document should give a clear definition of the terms it's going to use, and then stick consistently to those terms as defined.

BarryWhit
Senior III

STOne-32 wrote:

> Indeed nowadays “resonators” are rarely used

 

So clearly the word "resonator" is not universally understood in this way.

 

I completely agree with the rest. Define your terms, Spinoza.

 

- If a post has answered your question, please acknowledge the help you received by clicking "Accept as Solution".
- Once you've solved your issue, please consider posting a summary of any additional details you've learned. Your new knowledge may help others in the future.