2021-08-31 8:58 AM
There is an inconsistency in RTC shadow register update frequency description. Some places in text mentions that shadow register update happens once every RTCCLK period:
34.3.5, 36.3.4: "Every RTCCLK periods, the current calendar value is copied into the shadow registers..."
34.3.10, 36.3.8: "The copy is performed every RTCCLK cycle."
And other place say that it actually happens every other RTCCLK cycle:
34.6.7, 36.6.3: "Calendar values (when reading from RTC_SSR, RTC_TR, and RTC_DR) are taken from the shadow registers, which are updated once every two RTCCLK cycles."
I assume that "every two RTCCLK cycles" is correct, because some other Reference Manuals state this consistently.
Solved! Go to Solution.
2021-09-27 8:31 AM
Hello @Stepan Martinek and welcome to the Community :)
The shadow registers are updated every ck_rtc cycle on RTC2_v2_0 and all versions after that.
I think it was "every two cycles" for v1.
So, "every two RTCCLK cycles" is wrong and should be “every RTCCLK cycle�?.
Hope this answer your question.
When your question is answered, please close this topic by choosing Select as Best.
Imen
2021-09-27 8:31 AM
Hello @Stepan Martinek and welcome to the Community :)
The shadow registers are updated every ck_rtc cycle on RTC2_v2_0 and all versions after that.
I think it was "every two cycles" for v1.
So, "every two RTCCLK cycles" is wrong and should be “every RTCCLK cycle�?.
Hope this answer your question.
When your question is answered, please close this topic by choosing Select as Best.
Imen
2021-09-27 10:03 AM
Hi Imen,
> So, "every two RTCCLK cycles" is wrong and should be “every RTCCLK cycle�?.
This means to fix virtually every STM32 RM, except RM0008, isn't it?
And also AN4759
(and yes, I still consider "modern feel and look" wrong.)
Also, AN4759 should mention in this very chapter the RTC v2 lock bug.
Jan
@Imen DAHMEN
2021-09-29 12:23 AM
Hello and thank you for clarification.
2021-09-30 12:58 AM
Thanks @[waclawek.jan] for your feedback.
I have escalated this issue to the appropriate Owner for further check all impacted docs and take the action for correction.
Imen
2021-09-30 2:41 AM
Thanks, Imen!
Jan
2024-02-12 4:46 AM