cancel
Showing results for 
Search instead for 
Did you mean: 

Configuration Request TIM1 based PWM generation with DMA ,the TIM1 will triger the ADC with DMA

thannara123
Senior

Hello ,

 

I want to make 4 channel PWM signal using TIM1 (with complimentory also)  .While the TIM1 is used to triger the ADC to get sample .

I am getting the pwm wave , But  ADC is not triggering or not working . What configuration i require  

 

Please see more details below  

 

I am Trying to generate 2 Channel PWM Genertaion [ CH1 CHN and  PWD Generation CH2CH2N ] from  DMA  Buffer .

   HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, (uint32_t *)sin_table, 160);

    HAL_TIMEx_PWMN_Start_IT(&htim1, TIM_CHANNEL_1);

    HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_2, (uint32_t *)sin_table, 160);

    HAL_TIMEx_PWMN_Start_IT(&htim1, TIM_CHANNEL_2);

Configuration as follows 

Screenshot 2024-04-26 at 2.44.46 PM.pngScreenshot 2024-04-26 at 2.45.24 PM.png

Screenshot 2024-04-26 at 2.47.09 PM.png

While PWM generation am trying to  TIM1 is  to triger the  ADC 

Screenshot 2024-04-26 at 2.52.27 PM.png

 

The ADC configured as follows 

HAL_ADCEx_Calibration_Start(&hadc);

HAL_ADC_Start_DMA(&hadc, (uint32_t *)ADC_RES, 200);

Screenshot 2024-04-26 at 2.56.13 PM.png

Screenshot 2024-04-26 at 2.56.59 PM.png

Screenshot 2024-04-26 at 3.02.40 PM.png

Am here attached the main.c file 

 

@AScha.3 

 

 

 

 

 

 

 

3 REPLIES 3
AScha.3
Chief III

Hi,

just what i see now : not enable continuous..

adc...dma:

AScha3_0-1714128886214.png

+

see my use case : tim8 -> trigger -> adc (with dma )

tim8:

AScha3_2-1714129104065.png

 

adc:

AScha3_1-1714129025120.png

 

start in main.c : (but i use not circular dma here, doing just one 512 sample-shot.)

 

retval = HAL_ADC_Start_DMA(&hadc1, (uint32_t *) &sampels[nu][0], 512);

while(HAL_DMA_GetState(&hdma_adc1) > HAL_DMA_STATE_READY) {};	// wait for ready

 

If you feel a post has answered your question, please click "Accept as Solution".
thannara123
Senior

I tried DMA continuous. request turned off ?

If circular mode turn off is it restart from zero after 512 ?

Other configuration is correct in my case ?

 

In the below code i didnt get the trigger in GPIOC Pin4  what is the wrong with me ?

void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)

{      if (htim->Instance == TIM1) 

            { t occurs HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_4);

             }

}

 

>I tried DMA continuous. request turned off ?

Just try it. 

>If circular mode turn off is it restart from zero after 512 ?

Yes, without circular mode : just filling the array one time. (Same as "one shot" on a DSO .)

Next dma start...same again.

>Other configuration is correct in my case ?

Hmmm...try. If you want continuous operation, then circular mode is correct; you have to use/copy data then in half/full callbacks - or just let it run. Only one dma-start needed here, it will loop always/endless and fill the array.

If you feel a post has answered your question, please click "Accept as Solution".