Skip to main content
Associate III
September 18, 2024
Solved

Communication between Nucleo-F411RE and Raspberry Pi using ST-Link VCP

Hello, i am using STM32F411RE with raspberry pi 4. i want to communicate rasp with stm32 through usb cable from pi to CN1 of stm32. i want the communication both ways. could you please tell me how to do it?
Thank you in advance.

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
September 18, 2024

@suhfi wrote:

okay, we enable the usart connectivity, how do we connect them


The UART connection is carried over the USB link.

  • Whatever is sent from the UART on the STM32 will be received on the host via its Virtual COM Port; eg, COM13 on your PC or /dev/ttyACM0 on my Raspberry Pi
  • Whatever is sent to the Virtual COM Port on the host (eg,COM13 or /dev/ttyACM0) will be received at the UART on the STM32.

@suhfi wrote:

but i can say the stm32 nucleo board and raspberry pi 4 has voltage differences 


That's all taken care of by the USB link

 


@suhfi wrote:

 i dont want jumper pins to be connected. 


The default configuration of the Nucleo board is that USART2 of the stm32f411re microcontroller chip is connected to the ST-Link's VCP - you shouldn't need to modify any links.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

26 replies

Andrew Neil
Super User
September 18, 2024

You need to give more details:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 


@suhfi wrote:

CN1 of stm32.


STM32 is just the microcontroller chip - it has no CN1

Are you talking about a Nucleo-F411RE board ?

 

AndrewNeil_1-1726652761299.png

https://www.st.com/en/evaluation-tools/nucleo-f411re.html

In which case CN1 is the ST-Link connector.

So you're wanting to use the ST-Link's VCP (Virtual COM Port) for UART communication with your RPi?

https://www.st.com/resource/en/user_manual/um1724-stm32-nucleo64-boards-mb1136-stmicroelectronics.pdf#page=25

Does the ST-Link's VCP show up on the RPi when you plug it in?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
September 18, 2024

Hello @suhfi ,

The title needs to provide a summury of your request. Putting "Communication" as a title doesn't give a clear information about your request. The title needs also to be concise. I'm updating your title then ..

I invite you to read these tips on how to post in this community.

Thank you for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
September 18, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
suhfiAuthor
Associate III
September 18, 2024

yes, i want to know how to do the communication between stm32f411re and raspberry pi 4 using usb cable connected to raspberry pi 4 and CN1 of stm32f411re. how can i do that.
i have seen many blogs but none of them are clear how to do thatt.

i want two way communication between them.

mƎALLEm
ST Technical Moderator
September 18, 2024

You need that Raspberry detects your STLINK as VCP (Virtual Comport).

So it's a Linux stuff not related to the STM32:

So to me the subject is more: "How to detect and use Serial Ports under Linux"

See these links:

https://www.cyberciti.biz/faq/find-out-linux-serial-ports-with-setserial/

https://thelinuxforum.com/articles/752-how-to-list-serial-ports-on-linux

...

I think you need to get something like: ttyUSB

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
September 18, 2024

OK, I just dug out an RPi and Nucleo board, and tried it.

Before plugging-in the Nucleo board:

AndrewNeil_0-1726661247833.png

After plugging-in the Nucleo board, I get the pop-up for the MSC:

AndrewNeil_1-1726661305479.png

and there is a new /dev/ttyACM0:

AndrewNeil_3-1726661502738.png

 

@suhfi so here,  the /dev/ttyACM0 is the ST-Link's Virtual COM Port on the Raspberry Pi;  you use it just as you would use any other "COM port" (ie, /dev/tty... device) on a Linux system - there is nothing special or specific to STM32 as far as Linux & the Raspberri Pi are concerned.

The actual /dev/tty... device assigned may be different - just like you get different COMxx: numbers in Windows - so use the above method to discover what device is created on your particular system.

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.