2020-02-25 2:17 AM
I'm using the FMC of the STM32H743 to drive a 16-bit 8080-bus LCD controller.
I've tried using DMA, MDMA and a CPU-loop to transfer data to the 8080-bus, via the FMC.
The transfer frequency does not depend on whether DMA, MDMA or CPU-loop is used. This make me think that the DMA/MDMA/CPU-loop is not the limiting factor.
At a 480MHz FMC clock, the transfer happens at just 1.6MHz, giving me only 20fps on a 16-bit colour 320x240 LCD.
At a 240MHz FMC clock, the transfer happens at just 0.8MHz, and so on at slower speeds.
I've also tried reducing the various setup and hold times to 1 and 0 cycles, but this has (surprisingly) not affected the waveform on the 8080-bus.
My (Cube-MX generated) FMC initialisation code is:
/* FMC initialization function */
static void MX_FMC_Init(void)
{
/* USER CODE BEGIN FMC_Init 0 */
/* USER CODE END FMC_Init 0 */
FMC_NORSRAM_TimingTypeDef Timing = {0};
FMC_NORSRAM_TimingTypeDef ExtTiming = {0};
/* USER CODE BEGIN FMC_Init 1 */
/* USER CODE END FMC_Init 1 */
/** Perform the SRAM1 memory initialization sequence
*/
hsram1.Instance = FMC_NORSRAM_DEVICE;
hsram1.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
/* hsram1.Init */
hsram1.Init.NSBank = FMC_NORSRAM_BANK2;
hsram1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
hsram1.Init.MemoryType = FMC_MEMORY_TYPE_SRAM;
hsram1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;
hsram1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;
hsram1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
hsram1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
hsram1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
hsram1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;
hsram1.Init.ExtendedMode = FMC_EXTENDED_MODE_ENABLE;
hsram1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;
hsram1.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;
hsram1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;
hsram1.Init.WriteFifo = FMC_WRITE_FIFO_DISABLE;
hsram1.Init.PageSize = FMC_PAGE_SIZE_NONE;
/* Timing */
Timing.AddressSetupTime = 3;
Timing.AddressHoldTime = 15;
Timing.DataSetupTime = 4;
Timing.BusTurnAroundDuration = 1;
Timing.CLKDivision = 16;
Timing.DataLatency = 17;
Timing.AccessMode = FMC_ACCESS_MODE_A;
/* ExtTiming */
ExtTiming.AddressSetupTime = 3;
ExtTiming.AddressHoldTime = 15;
ExtTiming.DataSetupTime = 4;
ExtTiming.BusTurnAroundDuration = 1;
ExtTiming.CLKDivision = 16;
ExtTiming.DataLatency = 17;
ExtTiming.AccessMode = FMC_ACCESS_MODE_A;
if (HAL_SRAM_Init(&hsram1, &Timing, &ExtTiming) != HAL_OK)
{
Error_Handler( );
}
HAL_SetFMCMemorySwappingConfig(FMC_SWAPBMAP_SDRAM_SRAM);
}
The (Cube-MX generated) clock setup is:
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Macro to configure the PLL clock source
*/
__HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSE);
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 480;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 20;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_1;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SPI1|RCC_PERIPHCLK_USB
|RCC_PERIPHCLK_QSPI|RCC_PERIPHCLK_FMC;
PeriphClkInitStruct.PLL2.PLL2M = 2;
PeriphClkInitStruct.PLL2.PLL2N = 120;
PeriphClkInitStruct.PLL2.PLL2P = 8;
PeriphClkInitStruct.PLL2.PLL2Q = 2;
PeriphClkInitStruct.PLL2.PLL2R = 1;
PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_2;
PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOWIDE;
PeriphClkInitStruct.PLL2.PLL2FRACN = 0;
PeriphClkInitStruct.FmcClockSelection = RCC_FMCCLKSOURCE_PLL2;
PeriphClkInitStruct.QspiClockSelection = RCC_QSPICLKSOURCE_D1HCLK;
PeriphClkInitStruct.Spi123ClockSelection = RCC_SPI123CLKSOURCE_PLL;
PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_PLL;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Enable USB Voltage detector
*/
HAL_PWREx_EnableUSBVoltageDetector();
}
How can I make the FMC on the STM32H743 transfer half-words faster than 1.6MHz, when driven with a 480MHz clock?
(I'd like to achieve 5MHz for 60fps.)
Solved! Go to Solution.
2020-02-25 5:50 AM
I've changed to using NE1 and continued using 0xC000 0000.
Now that I'm configuring (NE) bank 1 and using NE bank 1, I'm getting 5MHz with just a 48MHz FMC clock and the default timings and clock division.
Previously I was configuring the NE bank 2, but writing to the entirely unconfigured NE bank 1's address. The fact that it worked at all is surprising.
2020-02-25 3:05 AM
Check the timings...
You can try the following changes
Timing.CLKDivision = 8;
ExtTiming.CLKDivision = 8;
And see whether something happens.
2020-02-25 3:59 AM
@Mike_ST I tried that, but it didn't make any difference.
I think I may have spotted the cause of the problem, though I have not yet fixed it.
I have set :
hsram1.Init.NSBank = FMC_NORSRAM_BANK2;
but I am writing to 0xC000 0000. (When I wrote to 0x6000 0000, before swapping banks, I was getting spurious writes: https://community.st.com/s/question/0D50X00009XkWQE/stm32h743ii-fmc-8080-lcd-spurious-writes .)
I don't care about FMC's chip select, because the LCD is the only other thing on the bus, and its #CS is wired to GND.
I think that the problem is that I'm *configuring* NE bank 2 and then *using* NE bank 1 (by writing to 0xC000 0000).
(The definition of 4 "NE banks" within "FMC bank" 1 confuses me, as it's never clear which type of bank an argument is referring to.)
I will spend some time fixing the hard faults that changing NE2 to NE1 has caused.
Is the address 0xC000 0000 correct to write to NE bank 1 of FMC bank 1 after "HAL_SetFMCMemorySwappingConfig(FMC_SWAPBMAP_SDRAM_SRAM);"?
2020-02-25 5:25 AM
I don't know how addressing issues can influence timings.
Please check TABLE 147 in RM 0433, maybe that can help a bit.
HAL_SetFMCMemorySwappingConfig(FMC_SWAPBMAP_SDRAM_SRAM); will set BMAP[1:0]=01.
2020-02-25 5:50 AM
I've changed to using NE1 and continued using 0xC000 0000.
Now that I'm configuring (NE) bank 1 and using NE bank 1, I'm getting 5MHz with just a 48MHz FMC clock and the default timings and clock division.
Previously I was configuring the NE bank 2, but writing to the entirely unconfigured NE bank 1's address. The fact that it worked at all is surprising.
2020-02-25 5:51 AM
@Mike_ST Thanks for your help. Can you close this ticket please?
2020-02-25 5:58 AM
You are welcome.
I can't close topics myself, if you like you can flag it as answered, .