2024-12-05 3:10 AM - last edited on 2024-12-05 4:50 AM by mƎALLEm
From a previous question: https://community.st.com/t5/stm32-mcus-products/stm32h745-dac2-missing/td-p/750749
So I can get two independent analog outputs using STM32H745?
Solved! Go to Solution.
2024-12-05 4:01 AM
Yes you can. DAC channels are independent. See this thread: https://community.st.com/t5/stm32-mcus-products/independent-dac-channel-triggers-on-stmf3xx/td-p/436595
You can use also DMA for both channels.
2024-12-05 3:12 AM
Two channels means you can generate two analog outputs with the same DAC instance.
2024-12-05 3:40 AM
Can I get for example sine wave output with 1kHz frequency from DAC_OUT1 and 2kHz sine from DAC_OUT2 at same time?
2024-12-05 3:56 AM - last edited on 2024-12-05 3:59 AM by Andrew Neil
Merged from duplicate thread.
Hi,
Is it possible to have two independent analog outputs from STM32H745? For example 1kHz sine from DAC1_OUT1 and 2kHz sine from DAC1_OUT2 at same time using DMA?
2024-12-05 4:01 AM
Yes you can. DAC channels are independent. See this thread: https://community.st.com/t5/stm32-mcus-products/independent-dac-channel-triggers-on-stmf3xx/td-p/436595
You can use also DMA for both channels.