2020-11-13 1:29 AM
Hi, I've created a custom keyboard and so far all works good. I've just a problem: I want to use an OK button on the keyboard to copy the text edited to a text area in an other screen. I'm able to go to the other screen but when i do the second part of my goal, I've got errors. I think the problem is in the function getBuffer.
-This is the part in customkeyboard.cpp
void CustomKeyboard::okPressedHandler()
{
getBuffer(); // function to save the actual entered text
application().gotoScreen01ScreenNoTransition(); // if i use only this line the code work to change screeen
}
-Part in customkeyboard.hpp
virtual void getBuffer()
{
// implemented in screen02_00View.cpp
}
-Part in the screen where the keyboard is defined
extern Unicode::UnicodeChar keyboardBuffer[10];
void Screen02_00View::getBuffer() // added to manage the entered text from temperature keyboard
{
Unicode::UnicodeChar* buff = keyboard.getBuffer();
Unicode::strncpy(keyboardBuffer, buff, Unicode::strlen(buff) + 1);
}
-Part in screen.hpp
virtual void getBuffer(); //added to manage the keyboard entered text
-Part in the screen where I want to go when i pressed ok button and where i want to save the text edited
Unicode::UnicodeChar keyboardBuffer[10]; // at the beginning of the code
void Screen01View::updateScreen() // I've defined updateScreen from touchGFX
{
if(Unicode::strlen(keyboardBuffer) > 0)
{
memset(&BakeText3Buffer, 0, BAKETEXT3_SIZE);
Unicode::strncpy(BakeText3Buffer, keyboardBuffer, BAKETEXT3_SIZE - 1);
BakeText3Buffer[BAKETEXT3_SIZE-1] = '\0'; // make sure last index is null
BakeText3.invalidate();
}
}
Part in the screen01.hpp
virtual void updateScreen();
Could you please help me?
Thank you
This is my keyboard:
Solved! Go to Solution.
2020-11-16 9:05 PM
As the error mentions, CustomKeyboard::getBuffer() is undefined. It is because CustomKeyboard does not have the getBuffer() function. It's the Keyboard class that has it, not CustomKeyboard ;) CustomKeyboard does not inherit from the Keyboard class but only has a Keyboard object as an attribute.
So you need to define a getBuffer() function in your CustomKeyboard class to be able to call it from your ScreenView.
Something like :
Unicode::UnicodeChar* CustomKeyboard::getBuffer()
{
return keyboard.getBuffer();
}
Don't forget to declare it in the .hpp file as well.
The fact that both your CustomKeyboard and Keyboard variable have the same name is misleading. I suggest you to change your CustomKeyboard variable name to customKeyboard to avoid mixing them.
When your question is answered, please close this topic by choosing Select as Best.
/Alexandre
2020-11-13 9:39 AM
I see more as one bad idea in your code.
Unicode::UnicodeChar* buff = keyboard.getBuffer(); this try return pointer from void function and too empty function ???
void CustomKeyboard::okPressedHandler()
{
getBuffer(); this call member empty not screen func
2020-11-16 12:00 AM
Hello GCamb2,
Could you provide the errors you got ? This would be helpful to assess the issue.
In the future, I believe it is good practice to include the errors to your post in order for the community to be able to support you the best we can.
/Alexandre
2020-11-16 12:04 AM
Yes sure, these are the first time I use the community so any advice can be useful.
The error is the following:
TouchGFX/build/STM32F746-DISCO/TouchGFX/gui/src/screen02_00_screen/Screen02_00View.o: In function `Screen02_00View::getBuffer()':
/TouchGFX/gui/src/screen02_00_screen/Screen02_00View.cpp:28: undefined reference to `CustomKeyboard::getBuffer()'
collect2.exe: error: ld returned 1 exit status
make[2]: *** [TouchGFX/build/bin/target.elf] Error 1
gcc/Makefile:289: recipe for target 'TouchGFX/build/bin/target.elf' failed
gcc/Makefile:285: recipe for target 'generate_assets' failed
make[1]: *** [generate_assets] Error 2
../gcc/Makefile:47: recipe for target 'all' failed
make: *** [all] Error 2
Failed
Failed
Thanks
2020-11-16 9:05 PM
As the error mentions, CustomKeyboard::getBuffer() is undefined. It is because CustomKeyboard does not have the getBuffer() function. It's the Keyboard class that has it, not CustomKeyboard ;) CustomKeyboard does not inherit from the Keyboard class but only has a Keyboard object as an attribute.
So you need to define a getBuffer() function in your CustomKeyboard class to be able to call it from your ScreenView.
Something like :
Unicode::UnicodeChar* CustomKeyboard::getBuffer()
{
return keyboard.getBuffer();
}
Don't forget to declare it in the .hpp file as well.
The fact that both your CustomKeyboard and Keyboard variable have the same name is misleading. I suggest you to change your CustomKeyboard variable name to customKeyboard to avoid mixing them.
When your question is answered, please close this topic by choosing Select as Best.
/Alexandre
2020-11-17 12:47 AM
Or maybe you can on invoke keyboard assign directly BakeText3Buffer to keyboard. Then only need in ok click use if empty and invalíidate text...
Noone of getBuffer chaos.