2023-06-01 02:28 AM - edited 2023-11-20 04:14 AM
Hi,
I use ADC3 on STM32H7, I need to know (and set) what is sampling frequency.
I use 3 channels in 16 bits.
What I tried to calculate?
1) Tconv_time = 8.5(setable)+8.5(fixed for 16 bits) = 17 ADC clock cycles = 17/30Mhz = 566 ns
2) From this image I should have Fadc_ker_ck = 30 MHz, becase my CKMODE = 0b11, and adc_sclk = 480/2 = 240 MHz (HPRE=2) - so it is sys_clk/2
Form above the Tconv should be 17/30Mhz = 567 ns
What about sampling frequency? My PRESC in ADC3_CCR = 0b1010 (divide by 128)
So I should divide some_CLK/128. What is the some_CLK? Is it the Fadc_ker_ck = 30 MHz?? Then it would be 30Mhz/128 = 234,375 kHz = 4,266 usec
Experiments:
I use BDMA for continual ADC3 measurement, I converts 200 samples for each chanels (3) = 600 samples.
I can measure the conversion time for all 3 channels - it takes 34.82 ms.
=> It is 600samples/34.82 ms => 1sample/58usec
So:
So what I did wrong?
Thank you very much
Solved! Go to Solution.
2023-06-02 06:13 AM
So now it is solved.
everything above about Tconv (sampling time) is corect. And because the clock I used is adc_sclk, so no DIV in ADCx_CCR register has effect on sampling frequency - that was probably main mistake I did.
Then if 1 sample takes 566 ns, then when I measure on all 3 channels, so measure period of first channel is 566*3 ns. And no another div has effect on this period...
2023-06-01 04:05 AM
if i see it right way....
you set 30M div 127 -> 4,2 us clock (very slow...) x 17 adc cycl. -> 71 us
you see 58 us , what would be 4,2 us x 14 adc cyc. , maybe you set 2.5+8.5 = 11 and switching channels cost some extra time.
so at first use div 10 , not 128 , and check speed.
2023-06-01 05:24 AM - edited 2023-11-20 04:14 AM
When I set div (PRESC in ADCX_CCR) to 10:
Then I can measure that 600 samples takes 1.6 ms => 1samples/2.66 usec
But theoretically it should be: 30Mhz/10= 3Mhz => 333 nsec ?!?
When I measure only 1 channel - it also takes 2.66 usec - so no extra cycles are needed to switch channels!
Also I am not sure if Tconv is dependent on PRESC in ADC3_CCR. From datashet I think it is not dependant:
2023-06-01 05:48 AM - edited 2023-11-20 04:14 AM
>But theoretically it should be: 30Mhz/10= 3Mhz
it should be + it is so. 333ns * 8 adc cyc. -> 2.6us
the adc still needs some cycles at this clock, to do his job.
+
>From datashet I think it is not dependant:
my ds thinking different:
2023-06-01 05:57 AM
>it should be + it is so. 333ns * 8 adc cyc. -> 2.6us
where did you take 8 adc cycles?
2023-06-02 04:42 AM
why 333* 8 adc cycles? where is written it should be 8? did you just put it there so that it would come out :-) ?
2023-06-02 06:13 AM
So now it is solved.
everything above about Tconv (sampling time) is corect. And because the clock I used is adc_sclk, so no DIV in ADCx_CCR register has effect on sampling frequency - that was probably main mistake I did.
Then if 1 sample takes 566 ns, then when I measure on all 3 channels, so measure period of first channel is 566*3 ns. And no another div has effect on this period...