cancel
Showing results for 
Search instead for 
Did you mean: 

ADC-DMA configuration

johnjones
Associate II

I have 6 channels on ADC1 and 2 channels on ADC2. I need the first two channels of ADC1 to be sampled simultaneously with the two channels of ADC2. The sampling needs to be triggered by a timer and occur twice each time the timer triggers.

Here’s what I did: I set the ADC mode to dual regular simultaneous + alternate trigger mode and enabled DMA access mode. I enabled continuous DMA requests and set the DMA to normal mode (not circular), so the buffer is filled only once each time the timer triggers. I also set the buffer size to 16, so the ADC channels are sampled twice and then stop once the buffer is filled. After that, the system waits for the next timer trigger.

Am I missing something?

1 REPLY 1
SofLit
ST Employee

Hello,

You need always provide the MCU part number as they are different in features and architecture stand points.

Please review the tips on this link on how to ask questions in this community.

Thank you for your understanding.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: Be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.