2025-01-12 11:39 PM
void SystemClock_Config(void)
{
LL_FLASH_SetLatency(LL_FLASH_LATENCY_4);
while(LL_FLASH_GetLatency() != LL_FLASH_LATENCY_4);
#if 1
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);
#endif
LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SCALE1); //Low power mode
while(LL_PWR_IsActiveFlag_VOS() != 0);
#ifdef _CLOCK_HSE_VER
/* HSE configuration and activation */
LL_RCC_HSE_Enable();
while(LL_RCC_HSE_IsReady() != 1);
#endif
#ifdef _CLOCK_MSI_VER
/* MSI configuration and activation */
LL_RCC_MSI_Enable();
while(LL_RCC_MSI_IsReady() != 1);
#endif
/*LSI configuration and activation*/
LL_RCC_LSI_Enable();
while(LL_RCC_LSI_IsReady() != 1);
/* Main PLL configuration and activation */
#ifdef _CLOCK_HSE_VER
LL_RCC_PLL_ConfigDomain_SYS(LL_RCC_PLLSOURCE_HSE, LL_RCC_PLLM_DIV_1, 10, LL_RCC_PLLR_DIV_2);
#endif
#ifdef _CLOCK_MSI_VER
LL_RCC_PLL_ConfigDomain_SYS(LL_RCC_PLLSOURCE_MSI, LL_RCC_PLLM_DIV_1, 40, LL_RCC_PLLR_DIV_2);
#endif
LL_RCC_PLL_EnableDomain_SYS();
LL_RCC_PLL_Enable();
while(LL_RCC_PLL_IsReady() != 1);
/* Sysclk activation on the main PLL */
LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL);
while(LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_PLL);
/* Set APB1 & APB2 prescaler*/
LL_RCC_SetAHBPrescaler(LL_RCC_SYSCLK_DIV_1);
LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_2);
LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_1);
/* Set systick to 1ms in using frequency set to 80MHz */
/* This frequency can be calculated through LL RCC macro */
/* ex: __LL_RCC_CALC_PLLCLK_FREQ(__LL_RCC_CALC_MSI_FREQ(LL_RCC_MSIRANGESEL_RUN, LL_RCC_MSIRANGE_6),LL_RCC_PLLM_DIV_1, 40, LL_RCC_PLLR_DIV_2)*/
/* Update CMSIS variable (which can be updated also through SystemCoreClockUpdate function) */
LL_SetSystemCoreClock(80000000);
}
The above code is the clock setting code. But what I'm curious about is whether there is a difference between calling the PWR activation code and not calling it. First of all, we confirmed that it works even when there is no PWR activation code, but there are cases where a reset phenomenon occurs. If you know the answer, please let me know. The MCU is using STM32L452REY6TR.
2025-01-13 1:48 AM
Hello @treeset,
The reset issue that you're encountering could be due to improper voltage scaling, the line "LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SCALE1);" sets the voltage scaling to optimize power consumption, this configuration requires the power interface clock to be enabled.
Which part of code exactly you consider is PWR activation code?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-13 5:58 PM
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);
I think this code make power interface clock to be enabled.