Implement an netx-duo-http server on a STM32F429ZIT6 MCU that uses a POST to initialize parameters
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-12 3:29 PM
I am using STMicroelectronics.X-CUBE-AZRTOS-F4 and STM32CubeIDE to make an NetXDuo HTTP server serve a web page POST from the MCU. The sample: "rtos-docs/netx-duo/netx-duo-http/Chapter2" is a minimal implementation. It is not an ST project, and does not adequately explain how to load the HTML from FLASH (I know how to write the binary web page to FLASH.), but does detail the minimum HTTP server for the application. I read through the excellent STM paper: "How to implement a webserver in STM32 using NetXDuo" and reviewed the STM NX_WEBSERVER NUCLEO-F429ZI sample. I know how to write the binary web page to FLASH.
The literature said to use TIM6 as a Time base Source instead of SysTick. When I run the app, I get a hard fault in the entry to the SystemTimerThread, which seems to be automatically created. Does anyone know how to work around this fault?
I am simply looking for the "minimum" implementation of an HTTP server that will handle one POST, any suggestions?
- Labels:
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-14 3:04 PM
So you build this Nx_WebServer example and run it on the Nucleo STM32F429ZI board, and it faults?
Please start from the original project and try to get it "working" as is, before changing anything in the code (timers, html pages etc.). Then carefully compare it with the other non-ST project and merge only the needed differences, without disturbing netx and threadx "base".
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-13 12:04 PM
I can successfully serve a page and POST back to the server. I extract the values from the POST (they are all valid); now I try to write these values to flash. I selected Sector 19. Here is the simplest code I could find to save to flash: STM32F429ZIT6 MCU
#define FLASH_ADDRESS 0x080E0000
uint32_t myData = 1234;
void save_data(uint32_t Address,uint32_t data){
HAL_FLASH_Unlock();
FLASH_EraseInitTypeDef EraseInitStruct;
EraseInitStruct.NbSectors = 1;
EraseInitStruct.Sector = 19;
EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS;
EraseInitStruct.VoltageRange = FLASH_VOLTAGE_RANGE_3;
uint32_t PageError;
if (HAL_FLASHEx_Erase(&EraseInitStruct, &PageError) != HAL_OK) //Erase the Page Before a Write Operation
{
//return HAL_ERROR;
}
HAL_Delay(50);
HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD,Address,(uint64_t)data);
HAL_Delay(50);
HAL_FLASH_Lock();
}
No errors are thrown.
Can you think of a reason that this should not save a uint32_t value to 0x080E0000 ?
I have tried many more sophisticated versions and they don't work either.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-13 5:53 PM
If nothing works - time to return to the basics. Find a suitable flash programming example in the Cube package, build and run. Should work.