cancel
Showing results for 
Search instead for 
Did you mean: 

32F417 SPI running at half the speed it should

PHolt.1
Senior III

Hello,

I am using a chopped-down function from the Cube HAL code to talk to a serial FLASH. The original function has a mass of options which were checked at runtime - the usual thing for HAL code...

It's all working fine. SPI2, 21MHz (the fastest I can go with PCLK1=PCLK2=42MHz).

But testing the speed, I am seeing 600us time taken to read 512 bytes. The SPI speed limit should be about 200us. The actual time, obtained by waggling a pin, is 600us. Can anyone see anything obviously wrong with this code? As I say, it works perfectly.

// Used only for SPI2. Mode is always SPI_MODE_MASTER and 2LINE.
 
//__attribute__((optimize("O0")))
HAL_StatusTypeDef B_HAL_SPI_TransmitReceive(SPI_HandleTypeDef *hspi, uint8_t *pTxData, uint8_t *pRxData, uint16_t Size)
{
  uint16_t             initial_TxXferCount;
  uint32_t             tmp_mode;
  HAL_SPI_StateTypeDef tmp_state;
 
  /* Variable used to alternate Rx and Tx during transfer */
  uint32_t             txallowed = 1U;
  HAL_StatusTypeDef    errorcode = HAL_OK;
 
  /* Init temporary variables */
  tmp_state           = hspi->State;
  tmp_mode            = hspi->Init.Mode;
  initial_TxXferCount = Size;
 
  if (!((tmp_state == HAL_SPI_STATE_READY) || \
        ((tmp_mode == SPI_MODE_MASTER) && (hspi->Init.Direction == SPI_DIRECTION_2LINES) && (tmp_state == HAL_SPI_STATE_BUSY_RX))))
  {
    errorcode = HAL_BUSY;
    goto error;
  }
 
  if ((pTxData == NULL) || (pRxData == NULL) || (Size == 0U))
  {
    errorcode = HAL_ERROR;
    goto error;
  }
 
  /* Don't overwrite in case of HAL_SPI_STATE_BUSY_RX */
  if (hspi->State != HAL_SPI_STATE_BUSY_RX)
  {
    hspi->State = HAL_SPI_STATE_BUSY_TX_RX;
  }
 
  /* Set the transaction information */
  hspi->ErrorCode   = HAL_SPI_ERROR_NONE;
  hspi->pRxBuffPtr  = (uint8_t *)pRxData;
  hspi->RxXferCount = Size;
  hspi->RxXferSize  = Size;
  hspi->pTxBuffPtr  = (uint8_t *)pTxData;
  hspi->TxXferCount = Size;
  hspi->TxXferSize  = Size;
 
  /*Init field not used in handle to zero */
  hspi->RxISR       = NULL;
  hspi->TxISR       = NULL;
 
  /* Check if the SPI is already enabled */
  if ((hspi->Instance->CR1 & SPI_CR1_SPE) != SPI_CR1_SPE)
  {
    __HAL_SPI_ENABLE(hspi);
  }
 
  	/* Transmit and Receive data in 8 Bit mode */
 
    // The need for this initial byte is unknown
    if (initial_TxXferCount == 0x01U)
    {
      *((__IO uint8_t *)&hspi->Instance->DR) = (*hspi->pTxBuffPtr);
      hspi->pTxBuffPtr++;
      hspi->TxXferCount--;
    }
 
    while ((hspi->TxXferCount > 0U) || (hspi->RxXferCount > 0U))
    {
      /* Check TXE flag */
      if ((__HAL_SPI_GET_FLAG(hspi, SPI_FLAG_TXE)) && (hspi->TxXferCount > 0U) && (txallowed == 1U))
      {
        *(__IO uint8_t *)&hspi->Instance->DR = (*hspi->pTxBuffPtr);
        hspi->pTxBuffPtr++;
        hspi->TxXferCount--;
        /* Next Data is a reception (Rx). Tx not allowed */
        txallowed = 0U;
      }
 
      /* Wait until RXNE flag is reset */
      if ((__HAL_SPI_GET_FLAG(hspi, SPI_FLAG_RXNE)) && (hspi->RxXferCount > 0U))
      {
        (*(uint8_t *)hspi->pRxBuffPtr) = hspi->Instance->DR;
        hspi->pRxBuffPtr++;
        hspi->RxXferCount--;
        /* Next Data is a Transmission (Tx). Tx is allowed */
        txallowed = 1U;
      }
 
    }
 
    // Clear overrun flag in 2 Lines communication mode because received is not read
    // For 45DBxx the Init.Direction is always SPI_DIRECTION_2LINES and is set up in b_main.c
    //if (hspi->Init.Direction == SPI_DIRECTION_2LINES)
    //{
    	__HAL_SPI_CLEAR_OVRFLAG(hspi);
    //}
 
error :
  hspi->State = HAL_SPI_STATE_READY;
  return errorcode;
}

25 REPLIES 25
PHolt.1
Senior III

OK let me do more tests. The clock is definitely 21MHz but I can't exclude the possibility of *that bit of code* clocking stuff out with gaps, which is actually what I suspect.

You can easily exclude problems with ocassional lengthy delays caused by interrupts simply by writing a simple test program which does NOTHING but dump 512 bytes through SPI. It does not need to be meaningful for the sFLASH itself, you just observe the bus/timing.

JW

TDK
Guru

If you've measured it on a scope and there is no delay between bytes, and the rate is 21 MHz, then explain how you're "seeing 600us" transaction time. Those two facts are at odds and cannot both be true.

If you feel a post has answered your question, please click "Accept as Solution".
PHolt.1
Senior III

OK here we go. Spot on, the clock bursts have gaps of exactly 2/3 of the time.

The zoomed X axis is 200ns/div.

The waveform is ringing because I am probing the board without decent scope grounds.

Ignore other traces - they are irrelevant. Just the clock.

So what the hell is it waiting for during those 800ns? 2 whole byte periods.

0693W00000HrQnTQAV.png 

To recap, this is the code

0693W00000HrQxmQAF.png 

The title of the thread should say 1/3 not 1/2.

TDK
Guru

As we've been saying all along, the code cannot keep up with the data rate. Use DMA, higher optimization settings, or your own code to overcome the issue.

800ns is not a ton of time in terms of cycles. Did you specify your CPU clock rate anywhere in this post?

If you feel a post has answered your question, please click "Accept as Solution".
PHolt.1
Senior III

168MHz.

No, there is something in that code which is waiting exactly two byte periods.

Some timing issue, but I can't see it.

Maybe one of the two USART flags is not indicating the status until something else happens.

An example of this, not relevant here, is that you cannot (with most UARTs) get a "TX buffer empty" interrupt unless the TX buffer becomes empty, so you have to load a byte in there first (often that is done by a timer ISR).

> No, there is something in that code which is waiting exactly two byte periods.

Or executing code takes exactly two byte.

Have you read out and checked the SPI registers content? Do you have interrupts enabled on that SPI?

JW

PHolt.1
Senior III

Config function:

 
// Stripped down copy of this function
// Must not enable interrupts!
// Used only for SPI2
 
static void B_HAL_SPI_Init(SPI_HandleTypeDef *hspi)
{
 
	/* Init the low level hardware : GPIO, CLOCK, NVIC... */
	//  HAL_SPI_MspInit(hspi);
 
	GPIO_InitTypeDef GPIO_InitStruct = {0};
 
	/* Peripheral clock enable */
	__HAL_RCC_SPI2_CLK_ENABLE();
	__HAL_RCC_GPIOC_CLK_ENABLE();
	__HAL_RCC_GPIOB_CLK_ENABLE();
 
	/**SPI2 GPIO Configuration
	PC2     ------> SPI2_MISO
	PC3     ------> SPI2_MOSI
	PB10     ------> SPI2_SCK
	*/
	GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3;
	GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
	GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
	B_HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
	GPIO_InitStruct.Pin = GPIO_PIN_10;
	GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
	GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
	B_HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 
	hspi->State = HAL_SPI_STATE_BUSY;
 
	/* Disable the selected SPI peripheral */
	__HAL_SPI_DISABLE(hspi);
 
	/*----------------------- SPIx CR1 & CR2 Configuration ---------------------*/
	/* Configure : SPI Mode, Communication Mode, Data size, Clock polarity and phase, NSS management,
  	  Communication speed, First bit and CRC calculation state */
	WRITE_REG(hspi->Instance->CR1, (hspi->Init.Mode | hspi->Init.Direction | hspi->Init.DataSize |
                                  hspi->Init.CLKPolarity | hspi->Init.CLKPhase | (hspi->Init.NSS & SPI_CR1_SSM) |
                                  hspi->Init.BaudRatePrescaler | hspi->Init.FirstBit  | hspi->Init.CRCCalculation));
 
	/* Configure : NSS management, TI Mode */
	WRITE_REG(hspi->Instance->CR2, (((hspi->Init.NSS >> 16U) & SPI_CR2_SSOE) | hspi->Init.TIMode));
 
	#if defined(SPI_I2SCFGR_I2SMOD)
	/* Activate the SPI mode (Make sure that I2SMOD bit in I2SCFGR register is reset) */
	CLEAR_BIT(hspi->Instance->I2SCFGR, SPI_I2SCFGR_I2SMOD);
	#endif /* SPI_I2SCFGR_I2SMOD */
 
	hspi->ErrorCode = HAL_SPI_ERROR_NONE;
	hspi->State     = HAL_SPI_STATE_READY;
 
}

and this is the config:

// Config SPI2 for serial FLASH. This SPI channel runs as fast as it can.
// Note that the mode is always SPI_DIRECTION_2LINES even if a tx-only function is used e.g.
// B_HAL_SPI_Transmit.
 
static void KDE_Init_SPI2(void)
{
	hspi2.Instance = SPI2;
	hspi2.Init.Mode = SPI_MODE_MASTER;
	hspi2.Init.Direction = SPI_DIRECTION_2LINES;
	hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
	hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
	hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
	hspi2.Init.NSS = SPI_NSS_SOFT;
	hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;  // 21MHz; the max possible on SPI2
	hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
	hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
	hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
	hspi2.Init.CRCPolynomial = 10;
	B_HAL_SPI_Init(&hspi2);
}
 

No interrupts used in this code.

The mcu does not work out of source code.

Read out and check the relevant registers.

Write a simple test program which does NOTHING but dump 512 bytes through SPI. It does not need to be meaningful for the sFLASH itself, you just observe the bus/timing.

Insert the pin toggling into places within the Tx/Rx routine to see progress there.

Ultimately you want to use DMA. Not that it's without problems.

JW

Why can't Tx and Rx occur concurrently on symmetrical SPI bus?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..