cancel
Showing results for 
Search instead for 
Did you mean: 

If there are 2x internal DACs in the STM32F407XX MCUs, why does the STM32F407VG Discovery Board need an external DAC for audio applications?

YChu.7
Associate

I'm very new to the STM32, so sorry if this sounds stupid. As far as I could understand looking at the datasheets, the STM32F407XX has 2 DACs, but when embedded in the discovery board an external DAC (CS43L22) is used. Why is that?

2 REPLIES 2
Uwe Bonnes
Principal III

The internal DAC is noisier, but probably has better DC accuracy.

AvaTar
Lead

The CS43L22 DAC has higher resolution + less noise, and the chip adds headphone/speaker amplifiers.