2022-08-12 4:47 AM
Hello! I use B-G431-ESC1 inverter board. Type of motor is BLDC. When I rotate the motor manually with PWM off, there is no such position at which all hall sensors have a zero state, and it is right. I control the states of the sensors in debug mode.
After sending the start command and the start of movement, a zero combination of states appears. What could be the reason?
2022-10-06 3:33 AM
Ciao
It is possible that some noise glitches in the inputs make this reading wrong?
If it is the case you can try to implement a sort of digital filter reading the input more times before to ***** a low or high state.
Ciao
Gigi