2024-09-05 06:26 AM
Hello,
I have buy the NUCLEO-F302R8 board with the X-NUCLEO-IHM07M1 with the motor BR2807. Now I search for the library and code generation with STM32CubeMX. It is stand on the web page that is "Workflow supporting the STM32CubeMX GUI configurator". But I dosn't found the package for STM32CubeMX for this.
So I have download and install software X-CUBE-MCSDK. After starting of this I can select the correct hardware. But afte start the generation of the source code I become a error:
How can I solve it? Which package must I install in STM32CubeMX? I dosn't found a package for this.
Why can't I do this in STM32CubeMX?
Best regard, Bernd
2024-09-05 06:35 AM
Now I have check the same with the newer version X-CUBE-MCSDK-6. But here I become other errors during the generation:
2024-09-05 07:50 AM