2020-11-25 06:52 AM
Hi,
STM32 is working very well with the Windows application ST Motor Control Workbench Monitor. I want a interface document or manual for the serial communication which is happening between the STM32 and Control bench application. So that I can use the same communication protocol for master controller to interface with the BLDC driver controller instead of PC application.
Regards,
Nishanth M
Solved! Go to Solution.
2020-11-30 01:14 AM
Hello @NM,
You can find in the section 14 - Serial communication class overview of the User Manual 1052 STM32F PMSM single/dual FOC SDK v4.3, a dedicated part for the explanation of the MCSDK communication protocol.
Best Regards,
Antoine
2020-11-30 01:14 AM
Hello @NM,
You can find in the section 14 - Serial communication class overview of the User Manual 1052 STM32F PMSM single/dual FOC SDK v4.3, a dedicated part for the explanation of the MCSDK communication protocol.
Best Regards,
Antoine
2020-11-30 09:52 PM
Hi,
Thanks for your reply.... I got the document which I am looking for it.
Kind Regards,
Nishanth M