cancel
Showing results for 
Search instead for 
Did you mean: 

Required Manual for ST Motor Control Workbench Serial Interface Protocol

NM
Associate III

Hi,

STM32 is working very well with the Windows application ST Motor Control Workbench Monitor. I want a interface document or manual for the serial communication which is happening between the STM32 and Control bench application. So that I can use the same communication protocol for master controller to interface with the BLDC driver controller instead of PC application.

Regards,

Nishanth M

1 ACCEPTED SOLUTION

Accepted Solutions
AntoineC
ST Employee

Hello @NM​,

You can find in the section 14 - Serial communication class overview of the User Manual 1052 STM32F PMSM single/dual FOC SDK v4.3, a dedicated part for the explanation of the MCSDK communication protocol.

Best Regards,

Antoine

View solution in original post

2 REPLIES 2
AntoineC
ST Employee

Hello @NM​,

You can find in the section 14 - Serial communication class overview of the User Manual 1052 STM32F PMSM single/dual FOC SDK v4.3, a dedicated part for the explanation of the MCSDK communication protocol.

Best Regards,

Antoine

NM
Associate III

Hi,

Thanks for your reply.... I got the document which I am looking for it.

Kind Regards,

Nishanth M