2015-08-20 02:00 AM
Hi all,
I'm using Rowley Crossword IDE for MacOS and i have issue with compiling WEB FOC v4.1.0 project (import from Keil uVision project). Always when i try to build project i get this error: ''Can't open /PROJECT ADDRESS/BUILD CONFIGURATION/tmpdFtZGh for reading''. I used FOC v4.0 in Rowley CW and everything is OK. I checked access rights and seem's to be OK.Do you have any idea to solution? Thanks for your help and time Ondra2015-08-21 03:00 AM
I downloaded foc support file from link given below but it is not even opening.
http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF257936?icmp=pf257936_pron_pr_jan2015&sc=stsw-stm32100-pr2015-09-07 05:39 AM
Hi
I'm sorry We deliver the FW package with the support only for IAR and KEIL and we can't provide any help for other IDEs. Regards Gigi2015-09-07 05:43 AM
Ciao
Seems that now the link is working. Anyhow I suggest don't trust in hyperlink and prefer to search in the ST.com the P/N of the library that will be allways: STSW-STM32100 Ciao Gigi2021-06-27 10:54 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards