cancel
Showing results for 
Search instead for 
Did you mean: 

Auto incrementing a build number after each compile?

DiBosco
Senior II

Folks,

Is there a way to have a variable that is incremented each time the project is compiled? I can do this with Rowley Crossworks and it's really useful. I define and major and minor number then a build number gets incremented each time I compile and I can get those vlaues when I interrogate the device using a CLI.

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Bob S
Super User

Write your script/program to do whatever you need.  Then call it from the "pre-build" steps in the project's C/C++ Build settings.  Go to the project properties, then expand "C/C+ Build" on the left side, then click on "settings".  In the right side, click on the "Build Steps" tab.

View solution in original post

4 REPLIES 4
Bob S
Super User

Not built in to the IDE, though there are probably Eclipse add-ons that do this.  But you can add your own pre-build or post-build steps to do that.  Run a script file that mods the value inside a .c file.  I use the pre-build steps to insert the GIT commit hash into a variable, and the post-build steps to further process the hex/binary files (add CRC/SHA hashes, etc.).  Even on Windows, the IDE runs a Linux compatible shell so you have sed available.

DiBosco
Senior II

Hi, thanks for the reply.

When you say script, I'm guessing you mean you can get, say, a Python script to automatically run once you hit CTL-B, but before it actually does the compile?

 

If so, how do you implement the running of that script please? I can write the Python much easier than I can a bash script (I am running Linux so could run the latter at a push, although Python is likely better as some colleagues are unfortunate enough to have to run Windows.

 

Thanks!

Bob S
Super User

Write your script/program to do whatever you need.  Then call it from the "pre-build" steps in the project's C/C++ Build settings.  Go to the project properties, then expand "C/C+ Build" on the left side, then click on "settings".  In the right side, click on the "Build Steps" tab.

DiBosco
Senior II

Great, thanks very much. :)