2023-05-25 4:26 AM
Dear,
Microcontroler STM32H742 (stm32CubeIDE)
When i plug out and plug in device, this printing on UART_3:
ţ˙ţţţţţţţţüţüüüüüüüüüüüüüüüüüü
or:
ţ
NVT: FF FE FE
ţţ{FF}
i this problem was not watched on same device with stm32F205(Rowley crossworks).
I clear all buffer
char bufRcv[256] {'\0'}; but it nothing change
Could you have some solution
Many thanks
2023-05-25 4:30 AM
from time to time i have:
ţ
NVT: FF FE FE
ţţ{FF}
2023-05-25 5:30 AM
I try with delay, and i have less character but problem doesn't resolved, also big value delay
int main(void)
{
	assert(sizeof(Product) == 136);
	assert(sizeof(User) == 124);
	assert(sizeof(TareRec) == 60);
	assert(sizeof(WazenieRec) == 192);
	assert(sizeof(RaportSuszenia) == 264);
	assert(sizeof(PomiarSuszenia) == 68);
	assert(((sizeof(sParams) * 2) + 128) < PC::BUF_SIZE);//czy parametry mieszcza sie w buforze, zeby wyslac je w postaci HEX
 
	delay_ms(1000);
  HAL_Init();
//  HAL_Delay(1000);
  SystemClock_Config();
  PeriphCommonClock_Config();
  //HAL_Delay(100);2023-05-25 5:35 AM
> When i plug out and plug in
What exactly do you mean by "plug out and plug in"?
And what do you observe, mcu's UART_Rx (how do you observe that?), or mcu's UART_Tx connected in some way to a PC/terminal?
JW
2023-05-25 6:01 AM
I mean Plug the power cord to the mains.
I have RS232 on mainboard in computer and i use db9 cable.
problem is only after Plug the power cord to the mains.
I use Hercules RS232 terminal:
https://www.hw-group.com/software/hercules-setup-utility
I have open rs232 port in hercules and turn on and turn off device.
Device and computer is connect to the same power strip.
We watch the problem after plugin Zebra printer, when scale was plug the power cord to the mains, printer printing this string
2023-05-25 6:08 AM
You you are clearing
char bufRcv[256] {'\0'};
which sounds like a receive buffer.
What about the transmit buffer? That's doing the printf.
So your UART and buffer init and TX functions might be interesting to see.
2023-05-25 6:21 AM
Yes I clear all device and buffer rec and transmit sorry i past rec buffer, but to show how i do this, mayby better is use memset(localBuf, '\0', sizeof(localBuf));
char bufContinuesTransmition[32] {'\0'};
char buf[BUF_SIZE] {'\0'};
char printBuf[PC_PRINT_BUF_SIZE] {'\0'};
static char localBuf[50] {'\0'};
We use c11 and c++11 in this project.
2023-05-25 6:23 AM
//------------------------------------------------- First plug the power cord to the mains --------------------------------
ţ
NVT: FF FE FE
ţţţţţţţţţüüţüüüüüüüţüüüţü
//------------------------------------------------- Second plug the power cord to the mains -------------------------
ţ
NVT: FF FE FF
ţţţţţţţ˙ţţ
//------------------------------------------------- 3 plug the power cord to the mains -------------------------------
ţ˙ţţţţţţüüüüüüüüüüüüüüüüüüüü
//------------------------------------------------- 4 plug the power cord to the mains -------------------------------
ţ˙ţţţţţţüüüüüüüüüüüüüüüüüüüüţ˙ţ
NVT: FF FE FE
ţţţţţţţţüţüţüţüţüţü
NVT: FF FC FF
ü
//------------------------------------------------- 5 plug the power cord to the mains -------------------------------
ţ˙ţţţţţţţţţüüţüüüüüüüţüüüţüţ
2023-05-25 6:42 AM
You are working with hardware, so you cannot just assume that thrwoing out printf / cout gives you what you want.
There must be some kind of hardware linking functions, something like this, so the weak _write is linked to actual hardware with Uart3DmaTx():
/* printf uses syscall function "_write()",
 * which is declared as __weak,
 * replace it with uart output function
 */
int _write(int file, char *data, int len)
{
	/* printf to UART */
	if( 0 == Uart3DmaTx((uint8_t *)data, len, 0) ) return len;
	return 0;
}
 2023-05-25 6:55 AM
//**************************************************************************************
UART_3 Com1;
UART_HandleTypeDef huart3;
DMA_HandleTypeDef hdma_usart3_tx;
//--------------------------------------------------------------------------------------
void UART_3::Init()
{
__HAL_RCC_DMA1_CLK_ENABLE();
//koniguracja portow oraz dma nastepuje w HAL_UART_MspInit
ConfigureUsart();
HAL_NVIC_SetPriority(DMA1_Stream3_IRQn, 3, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream3_IRQn);
/* Peripheral interrupt init */
HAL_NVIC_SetPriority(USART3_IRQn, 2, 0);
HAL_NVIC_EnableIRQ(USART3_IRQn);
__HAL_UART_ENABLE_IT(&huart3,UART_IT_RXNE);
}
//--------------------------------------------------------------------------------------
//--------------------------------------------------------------------------------------
void UART_3::ConfigureUsart()
{
uint16_t parity = DecodeParity(Params.Com1_Parity);
huart3.Instance = USART3;
huart3.Init.BaudRate = DecodeBaudrate(Params.Com1_Baudrate);
huart3.Init.WordLength = (parity == PARITY_NONE) ? UART_WORDLENGTH_8B : UART_WORDLENGTH_9B;
huart3.Init.StopBits = UART_STOPBITS_1;
huart3.Init.Parity = parity;
huart3.Init.Mode = UART_MODE_TX_RX;
huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart3.Init.OverSampling = UART_OVERSAMPLING_16;
huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart3) != HAL_OK) Error_Handler();
if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK) Error_Handler();
if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK) Error_Handler();
if (HAL_UARTEx_DisableFifoMode(&huart3) != HAL_OK) Error_Handler();
}
//--------------------------------------------------------------------------------------