2020-11-12 09:55 AM
Hi
I have designed a board based on evspin32f0602 single shunt foc.
When I am using the same value of shunt resistor as the event spin board the motor runs normally
But I want to increase the load capacity to 16 amps
So what all changes i need to do beside shunt resistor. I have used .025 ohm as shunt resistor .
But now every time I turn on the motor it shows over load.
Is there any other resistor i have to change.
Thanks.
2020-11-24 03:03 AM
Hello Fkadr.1,
The original EVSPIN32F0602S1 board is limited to 8.5 Apeak.
In its User's Manual (UM2629), it provides you with chapter 6.3 on How To modify HW about the Overcurrent detection and Current sensing measurement. In particular, it informs about the few resistors to change according to the given formula.
Then, you have to make sure that your FW configuration is matching this new HW configuration. The MC Workbench software tools will help you to do that (Cf. the Current Sensing and the Overcurrent Protection blocks).
Best Regards.
2021-05-09 09:47 AM
2021-05-09 10:11 AM
I have solved all my queries and made my own board with higher amp rating.
thanks for your response
2021-05-09 10:12 AM
This is all you will need to operate the motor.But once you start playing with the software you will be accurately operate motor.
2021-05-09 10:55 AM
Many of Thanks for update...
@Fkadr.1 (Community Member)
1) Means these 10 parameters (as attached) is sufficient to spin the motor ? Rest should be default in mcsdk 5.4.6 ?
2) How to choose PWM Frequency and Execution Rate ? According to Motor Parameter ?
Any other suggestions ...
--
Karan