cancel
Showing results for 
Search instead for 
Did you mean: 

I need to profile a motor for a drone. Profiling with or without propeller?

Orso
Associate III

Hello,

I need to profile a motor to be used in a drone. I can profile it sussefully without and also with propeller on, but wich is the correct way to profile it? And why?

Thanks

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Super User

The relevant environment for performance is with a propeller attached because that is the intended/target configuration. Knowing how it performs without one is of dubious value.

If you feel a post has answered your question, please click "Accept as Solution".
Javier1
Principal

what software are you using for profiling? and what size is your motor?

hit me up in https://www.linkedin.com/in/javiermu%C3%B1oz/

I'm using ST motor profiler. The motor is a Protronik 2810, 1000KV, 25Apk, with a 3 cell battery (11.1V) and a 10x5 inches propeller (graupner e-prop).