@GRINA.1 ,As indicated into our User's Manual and the dedicated Application Notes applied to each topology, the standard library shall be selected as well ;-).FYI, it brings the DPC_Miscellaneous (header and source) files and few others available fo...
Dear @victagayun We are confident there is misusage of the pack. So, we would like to help you to get it right.Please, could you clarify the following information to start-up understanding your trouble:1/ HW configuration : 1.1/ ioc file used ? ...
Dears,Because behavior was different when using STM32CubeMX v6.6.1 and v6.7.0, we have issued a new X-Cube-DPower patch version (v1.0.2) for you. The previous problem existing with STM32CubeMX v6.7.0 is now solved, the "DCDC_Control_layer.c" file is ...
Dear CBrom,As far as I understand your trouble, I can see two ways getting the example source files from our MC SDK.1st one is to generate the example for another IDE, like EWARM.2nd one is to update the example like you do for steps 1) to 3), then t...
Dear CBrom,About the 6-steps example generation, please note that we have issued a new MC SDK 5.Y.2 which corrects few troubles. We recommend to use it from now. However, as it is only examples, you won't be able to use the MC WorkBench to make any c...