cancel
Showing results for 
Search instead for 
Did you mean: 

NEW X-CUBE-MCSDK version 5.4.4 available

Claire O.
ST Employee

Dear all,

We are pleased to announce that a new MCSDK release is now avalable at:

https://www.st.com/en/embedded-software/x-cube-mcsdk.html

Main updates of this release are:

  • new dual motor board STEVAL-CTM010V1 for PFC with STM32F3
  • workaround to palliate STM32G4 cut2.2 injected ADC conversion issue
  • And many bug fixes ( Position control, ST Motor Profiler, ST MC Workbench pin assignments, H7 example...).

All details are available in the Release Notes.

Thanks for using our products!

4 REPLIES 4
Ivan FILYAEV
Associate II

Dears,

There is declared Support for PFC on STM32F3 (Dual motor demo boardSTEVAL-CTM010V1), but during simulation this configuration in ST MC Workbench -v.5.4.4 there appear warning "The PFC is not supported in the FW for SDK5.x.x. except for SDK for 'STMF103 High Density'. All parameters will be disabled".

Should we count on STM32F3 PFC FW support in next SDK releases?

Claire O.
ST Employee

​Dear Ivan,

PFC for STM32F3 is already here, accessible from the example project list ( named STEVAL-CTM010V1 dual drive with PFC).

The warning popping should be removed... sorry. (and thanks for warning us!)

best regards,

Claire

MMa.1893
Associate III

why need require mcsdk-full version for every time when it get update?

​Dear customer,

There is a restriction of our downloading tools. We already reported this is a problem and are sorry about the situation.

Thanks and best regards,

Claire