cancel
Showing results for 
Search instead for 
Did you mean: 

Updating motor mechanical parameters : Inertia and friction

EDokm
Associate III

I am trying to control a 24V PMSM type motor using ST Motor Control Workbench version 6.3.1 with the FOC.

I have run Motor Profiler and then gotten the electrical and mechanical parameters.

I have three questions and can anybody help/answer them?

  1. I am running Motor Profiler without load? Am I doing correct?
  2. When creating a project using Motor Control Workbench, do I need to update the inertia and friction coefficients in the motor stage depending on the load (please see attachment)? If the answer is no, where should I include the inertia and friction of the load in the project?
  3. May I measure PMSM type motor inertia and friction coefficients with load? If yes, how can I do it?

Thanks in advance.

1 ACCEPTED SOLUTION

Accepted Solutions
GMA
ST Employee

Hello @EDokm,

You can profile your motor alone. In this case, once loaded, speed/torque regulator PID gain tuning has maybe to be done.
You can also profile the motor loaded if the profiler sequence isn’t a risk in your case (gear box or fan use case for example).

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

View solution in original post

1 REPLY 1
GMA
ST Employee

Hello @EDokm,

You can profile your motor alone. In this case, once loaded, speed/torque regulator PID gain tuning has maybe to be done.
You can also profile the motor loaded if the profiler sequence isn’t a risk in your case (gear box or fan use case for example).

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA