cancel
Showing results for 
Search instead for 
Did you mean: 

Best evaluation kit for Foc motor control

GFont.2
Associate

Hi,

I'm working in the robotic field and I want to learn more about the solutions provided by st for custom brushless motor control. I want to include the st motor control workbench, to generate the control code, in my workflow. I checked online and there are two very interesting evaluation kit that can be used to start using the stspin32f0 microcontroller that could be the perfect solution for our needs: steval-spin 3201 and the evalkit-robot-1. The last one has the advantages to have also the Maxon motor integrated and the Modbus communication implemented. However I want to use the st motor control workbench to try the motor profiler, to try changing the motor control parameters and modalities. It is possible to use the evalkit-robot-1 with the motor control workbench or I must use only the provided firmware?

Thank you in advance

Andrea Fontanelli

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Laurent Ca...
Lead II

Dear @GFont.2​ 

Do you have still this problem to solve?

Best regards

Laurent Ca...

Laurent Ca...
Lead II

Dear @GFont.2​ 

I guess you don't have to solve this problem anymore, therefore I consider this post closed.

If not, feel free to reopen it by posting a new answer.

Best regards

Laurent Ca...