2020-04-29 12:15 AM
When I try to open a .ioc file it shows a msg: MotorControl files not found.
Does it mean that it is missing any library or some other files related to that .ioc project?
2020-04-29 10:08 PM
Hello @Haward_SMA
Please try with this steps:
You already need a well-named directory in the STM32Cube repository :
Generally speaking: MCSDK_vX.Y.Z..
In this directory, you will have to copy the MotorControl directory found in the MCSDK installation:
and have the following content in the tree structure:
Best regards,
Nesrine
2020-04-29 11:55 PM
Hi @Nesrine.JLASSI , thank you very much for your help.
seems such motor control folder already in place
But still same issue.
And to make it worst, now have another problem, in a early stage.,
The file that I am trying to open is an example from ST website:
when opening the .ioc file, now it is showing an error that is missing a FW for F0.
But, as we can see on the first picture, I have the most updated FW.
Then, choosing continue or migrate, it will generate the error that was the 1st reason for this post.
Regards.
2020-04-30 02:06 AM
Hi @Haward_SMA
Try to uninstall and then install the MCSDK.
Regards,
Nesrine
2020-05-06 07:39 PM
Hi @Nesrine.JLASSI , tks for your comments.
Sorry my late reply, we had a long holiday here :grinning_face: .
I did that, but the problem persists..
I will keep investigating the issue.
Regards
2020-05-09 01:05 AM
Hi @Nesrine.JLASSI today, I notice something interesting.
I saw that, somehow, during the installation, it was created 2 repository folders
One of them had the MCSDK folder and the motor control files and the other one hasn't.
Even after comping the MSCDK folder to the other one, still not working.
Do you have any other guess?
Regards
2020-05-11 12:46 AM
Hello @Haward_SMA
I don't understand what you're saying. Could you clarify please.
Best regards,
Nesrine
2020-10-14 01:28 PM
Dear @Haward_SMA
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-10-22 01:31 AM
@Haward_SMA
Hello,
Please, could you update the STM32CubeMx version to latest one (currently 6.0), as well as the F0 FW (but seems almost ok) ? Then, just make sure you are using it when generating the Motor Control Project ;-).
Best Regards,
PBo
2020-10-26 02:36 AM
Dear @Haward_SMA
Any news?
Best regards
Laurent Ca...