cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Pilot bug: Torque resets to zero

DMeie.2
Senior

I'm having following issue with the Motor Pilot that comes with the MCSDK 6.2.1 (V1.2.5).

I try to modify the Rev-up phase configuration.
Now when I write a torque value in any of the phases, this value resets to zero and is saved on the board (pressing "Read parameters" returns the zero values). If that happens, I cannot set it to any other value until I power-cycle the board, in which case it resets to the values predefined in firmware.

Any way to make this feature usable again?

14 REPLIES 14
Gael A
ST Employee

Hello DMeie.2,

Have you tried our latest MCSDK 6.3.0 release ? Can you confirm that you still experience the issue on the latest MotorPilot ?

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.

I was not aware there's a new MCSDK release.
I will give it a try and report back.

Is there a way to subscribe anywhere to get notified about new releases?

Hello @DMeie.2,

Does MCSDK 6.3.0 release solved your issue?
If not, please have a look at this post

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
DMeie.2
Senior

At least using the MotorPilot tool in version 6.3.0 did not fix this issue.
I'll wait for an updated version of it that hopefully implements the locales fix mentioned in the other thread.

have also the same problem with version 6.3.1...