2014-03-24 5:02 PM
Hi
The motor control SDK 3.4 provides me with an LCDProject, which I believe contains the binary for the communications interface to the Motor Control Workbench program. There doesn't seem to be any source code provided for this feature, and the MCWB program seems to offer no options for nominating the MCU USART or UART for use with that feature. Is there a way to customise that feature to use a different MCU USART/UART peripheral, or are we stuck with USART1? Thanks Luke #uasrt-mcwb-customise-serial2014-03-24 5:09 PM
Another question:
If I remap USART1 in my application, will the feature use the remapped pins, or does it reconfigure for USART1 on the default USART1 pins? Thanks2014-03-24 5:57 PM
Oh, it looks like my question is already answered in the manual.
See UM1052, chapter 9. Thanks Luke2014-03-31 1:06 AM
Yes Luke,
better to take a look at the UM first ;) I'm joke, feel free to ask Ciao Gigi2021-06-21 9:23 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards