cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Control Serial Interface - Change USART for MCWB

luke23
Associate III
Posted on March 25, 2014 at 01:02

Hi

The motor control SDK 3.4 provides me with an LCDProject, which I believe contains the binary for the communications interface to the Motor Control Workbench program.

There doesn't seem to be any source code provided for this feature, and the MCWB program seems to offer no options for nominating the MCU USART or UART for use with that feature.

Is there a way to customise that feature to use a different MCU USART/UART peripheral, or are we stuck with USART1?

Thanks

Luke

#uasrt-mcwb-customise-serial
4 REPLIES 4
luke23
Associate III
Posted on March 25, 2014 at 01:09

Another question:

If I remap USART1 in my application, will the feature use the remapped pins, or does it reconfigure for USART1 on the default USART1 pins?

Thanks

luke23
Associate III
Posted on March 25, 2014 at 01:57

Oh, it looks like my question is already answered in the manual.

See UM1052, chapter 9.

Thanks

Luke

Gigi
ST Employee
Posted on March 31, 2014 at 10:06

Yes Luke,

better to take a look at the UM first ;)

I'm joke, feel free to ask

Ciao

Gigi

Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards